Can't Run the S32R274 Radar RTM 1.0.0 Example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't Run the S32R274 Radar RTM 1.0.0 Example

跳至解决方案
2,063 次查看
qinglongshang
Contributor I

   I imported the S32R274 Radar RTM 1.0.0 Example into the S32DS for PA 2017.

pastedImage_1.png

   I builded it successfully, but after I ran the Z4 and Z7_0 Core, the tftp_client_write function in Z4 Core encountered an error. The Error Info is shown below.#@@@

pastedImage_2.pngThanks a lot.S32 Design StudioAutomotive MCUs / MPUs and Tools

标记 (2)
0 项奖励
回复
1 解答
1,887 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried the example - and for me is working normally - but I don't use any communication channel, only PE Micro. I tried to locate tftp.c file - but it is part of library. 

What is your scenario settings? 

Jiri

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,888 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried the example - and for me is working normally - but I don't use any communication channel, only PE Micro. I tried to locate tftp.c file - but it is part of library. 

What is your scenario settings? 

Jiri

0 项奖励
回复