Can't Run the S32R274 Radar RTM 1.0.0 Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't Run the S32R274 Radar RTM 1.0.0 Example

ソリューションへジャンプ
2,074件の閲覧回数
qinglongshang
Contributor I

   I imported the S32R274 Radar RTM 1.0.0 Example into the S32DS for PA 2017.

pastedImage_1.png

   I builded it successfully, but after I ran the Z4 and Z7_0 Core, the tftp_client_write function in Z4 Core encountered an error. The Error Info is shown below.#@@@

pastedImage_2.pngThanks a lot.S32 Design StudioAutomotive MCUs / MPUs and Tools

タグ(2)
0 件の賞賛
返信
1 解決策
1,898件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried the example - and for me is working normally - but I don't use any communication channel, only PE Micro. I tried to locate tftp.c file - but it is part of library. 

What is your scenario settings? 

Jiri

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,899件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried the example - and for me is working normally - but I don't use any communication channel, only PE Micro. I tried to locate tftp.c file - but it is part of library. 

What is your scenario settings? 

Jiri

0 件の賞賛
返信