CAN receive example code in S32DS not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN receive example code in S32DS not working

2,584 Views
laxmikanthindur
Contributor III

Hi All,
Attached image is my setup for CAN communication using DEVkit MPC5748G.
I am trying CAN receive example code (flexcan_receive_Z0_4) in S32DS.


But code is not working. So for more diagnosis I traced CAN signal using DSO.
I have observed CAN high and Low signal on CAN_H and CAN_L.
But there is no signal found on Rx pin (Between transceiver IC and MPC5748G controller).


My set up is working for transmit example code ( flexcan_transmit_Z0_4) .


Please help me to sort out this problem.

pastedImage_1.png

0 Kudos
Reply
1 Reply

2,466 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

This seems to be a similar issue to the one in thread https://community.nxp.com/message/1025113 .

Try adding a 120 ohm resistor between CAN_H and CAN_L.

Hope it helps,

Mike

0 Kudos
Reply