Building SPT Kernel library in S32DS. not found in path error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building SPT Kernel library in S32DS. not found in path error

1,878件の閲覧回数
User133
Contributor II

I am trying to build the SPT Kernel library and am meeting the following errors.

User133_0-1654872723851.png

I am following these instructions from the user manual.

To build the SPT kernels, open DesignStudio, import the .project file located at < rsdk_path >/SPT/SPT_kernels/project/< hw_arch >, then press 'Project -> Build All'. Alternately, each target can be selected and built individually (Project -> Build Configurations -> Set Active, then Project -> Build Project). After the build process is finished, the libraries will be located in < rsdk_path >/SPT/SPT_kernels/bin.

User133_1-1654873707200.png

How can I resolve the errors?

0 件の賞賛
返信
2 返答(返信)

1,852件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is your S32DS Version? 

0 件の賞賛
返信

1,846件の閲覧回数
User133
Contributor II

C:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\middleware\rsdk

 

This is the version. 

0 件の賞賛
返信