S32V234 M4 example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32V234 M4 example

1,165 Views
SagiSalomon
Contributor I

Hi,

I am able to build for M4 target with freeRTOS using an example provided by the development kit.

I wish to burn/copy the elf to the board itself and see it runs.

What is the procedure in order to do so? I didnt find any way to use the elf file for the M4.

I am able to connect to the board using serial and ssh (linux core) and boot sequence from A53 (default configuration).

No debugging tool.

Thanks,

0 Kudos
Reply
0 Replies