Build a project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,369件の閲覧回数
Anjalipurushothaman
Contributor III

While building a project , only one target option is enabled, which make to only debug the configration.

If I need to flash the program into target processor , which has to be selected . (PE Micro is not poping up in the Run configration window)

wheras while debigging , i can selecte PE Micro.

Since toolchain will be same for any target proessor, Hope anyone can provide solution to this.

0 件の賞賛
返信
1 解決策
6,302件の閲覧回数
Anjalipurushothaman
Contributor III

Yes, That is correct

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
6,334件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

Please correct me if I am wrong. 

What you are trying to do is flash your micro with your debugger, but you do not see the "release" option, you only see "debug"? Am I correct?

 

B.R.

VaneB

0 件の賞賛
返信
6,303件の閲覧回数
Anjalipurushothaman
Contributor III

Yes, That is correct

0 件の賞賛
返信