Build a project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Build a project

跳至解决方案
6,567 次查看
Anjalipurushothaman
Contributor III

While building a project , only one target option is enabled, which make to only debug the configration.

If I need to flash the program into target processor , which has to be selected . (PE Micro is not poping up in the Run configration window)

wheras while debigging , i can selecte PE Micro.

Since toolchain will be same for any target proessor, Hope anyone can provide solution to this.

0 项奖励
回复
1 解答
6,500 次查看
Anjalipurushothaman
Contributor III

Yes, That is correct

在原帖中查看解决方案

0 项奖励
回复
2 回复数
6,532 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

Please correct me if I am wrong. 

What you are trying to do is flash your micro with your debugger, but you do not see the "release" option, you only see "debug"? Am I correct?

 

B.R.

VaneB

0 项奖励
回复
6,501 次查看
Anjalipurushothaman
Contributor III

Yes, That is correct

0 项奖励
回复