Build a project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build a project

Jump to solution
6,335 Views
Anjalipurushothaman
Contributor III

While building a project , only one target option is enabled, which make to only debug the configration.

If I need to flash the program into target processor , which has to be selected . (PE Micro is not poping up in the Run configration window)

wheras while debigging , i can selecte PE Micro.

Since toolchain will be same for any target proessor, Hope anyone can provide solution to this.

0 Kudos
Reply
1 Solution
6,268 Views
Anjalipurushothaman
Contributor III

Yes, That is correct

View solution in original post

0 Kudos
Reply
2 Replies
6,300 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

Please correct me if I am wrong. 

What you are trying to do is flash your micro with your debugger, but you do not see the "release" option, you only see "debug"? Am I correct?

 

B.R.

VaneB

0 Kudos
Reply
6,269 Views
Anjalipurushothaman
Contributor III

Yes, That is correct

0 Kudos
Reply