Bootloader for MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader for MPC5744P

3,155 Views
chuluezhong
Contributor II

Is there no NXP produced bootloader for the MPC5744P like there is for the Kinetis range of processors?

MCU Bootloader|NXP

Labels (1)
0 Kudos
Reply
2 Replies

2,779 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

There is RAppID Bootloader. You can download it from RAppID Boot Loader Utility. It is located on the product page for RAppID Initialization for Power Architecture|NXP.

Hope it helps,

Mike

0 Kudos
Reply

2,779 Views
chuluezhong
Contributor II

Hello Mike,

The RAppID BL utility requires first loading a rbf file onto the board (which I guess is the bootloader itself) which is how the utility talks to the MCU to perform the download. This seems to behave as it should for model based design applications, however I cannot get this to work for downloading applications over CAN.

Outlook <https://aka.ms/ghei36> for<https://aka.ms/ghei36> Android<https://aka.ms/ghei36> herunterladen

Von: mikedoidge

Gesendet: Montag, 9. Juli, 22:22

Betreff: Re: - Re: Bootloader for MPC5744P

An: Chulue Zhong

NXP Community

Re: Bootloader for MPC5744P

reply from Mike Doidge in S32 Design Studio - View the full discussion

Hello,

There is RAppID Bootloader . You can download it from RAppID Boot Loader Utility . It is located on the product page for RAppID Initialization for Power Architecture | NXP .

Hope it helps ,

Mike

Reply to this message by replying to this email, or go to the message on NXP Community Start a new discussion in S32 Design Studio by email or at NXP Community Following Re: Bootloader for MPC5744P in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos
Reply