Basic example project file for GHS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Basic example project file for GHS

2,697件の閲覧回数
leekate-b45752
NXP Employee
NXP Employee

Hello, 

Could I get an basic example project file for GHS with S32K14x? 

Best regards,

Kate Lee

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,528件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Kate,

You will first need to contact Green Hills to get the Eclipse Neon compatible plug-in. Then, after you install the plug-in, you should be able to use the New Project from Example wizard to see the Hello World example included in the SDK. Alternatively, you could use the New Project Wizard to create an empty project.

Best Regards,

Mike

0 件の賞賛
返信

2,528件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Kate, 

unfortunately I don't have any GHS examples for S32K144 - hope that someone on community will share something. 

Jiri 

0 件の賞賛
返信