BCC_S32K144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BCC_S32K144

20,572 次查看
rajesh1
Contributor I

When i am importing BCC(battery cell controller) example in s32 design studio it showing  messege: kinetis 

SDK SDK_s32k1xx_15 is not installed. screenshot is attached in attachment.can u help me out to install 

kinetis SDK SDK_s32k1xx_15.

标记 (3)
0 项奖励
回复
5 回复数

20,402 次查看
rajesh1
Contributor I

how to install this??

0 项奖励
回复

20,402 次查看
raresvasile
NXP Employee
NXP Employee

Hi,

Please install RTM 3.0.0 from: https://www.nxp.com/lgfiles/updates/S32DS/S32DS_ARM_v2018.R1_UP9.zip 

Thank you,

Rares

0 项奖励
回复

20,284 次查看
Kallappa
Contributor III

Hello,


I am also facing the same issue regarding the kinetes SDK . as you suggested I downloaded the SDK but not be able to include or add to the S32DS so it will really helpful if you help here.

Thanks in Advance.

0 项奖励
回复

20,272 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is your S32DS Version? 

 

Jiri

0 项奖励
回复

19,611 次查看
Zyuan17
Contributor III
Hi, I encountered the same problem. Do you have a direct download link to the SDK_s32k1xx_15? I am currently using S32K142+MC33771C.
0 项奖励
回复