BCC_S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BCC_S32K144

20,569 Views
rajesh1
Contributor I

When i am importing BCC(battery cell controller) example in s32 design studio it showing  messege: kinetis 

SDK SDK_s32k1xx_15 is not installed. screenshot is attached in attachment.can u help me out to install 

kinetis SDK SDK_s32k1xx_15.

Tags (3)
0 Kudos
Reply
5 Replies

20,399 Views
rajesh1
Contributor I

how to install this??

0 Kudos
Reply

20,399 Views
raresvasile
NXP Employee
NXP Employee

Hi,

Please install RTM 3.0.0 from: https://www.nxp.com/lgfiles/updates/S32DS/S32DS_ARM_v2018.R1_UP9.zip 

Thank you,

Rares

0 Kudos
Reply

20,281 Views
Kallappa
Contributor III

Hello,


I am also facing the same issue regarding the kinetes SDK . as you suggested I downloaded the SDK but not be able to include or add to the S32DS so it will really helpful if you help here.

Thanks in Advance.

0 Kudos
Reply

20,269 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is your S32DS Version? 

 

Jiri

0 Kudos
Reply

19,608 Views
Zyuan17
Contributor III
Hi, I encountered the same problem. Do you have a direct download link to the SDK_s32k1xx_15? I am currently using S32K142+MC33771C.
0 Kudos
Reply