Attach to running target keeps resetting mcu

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Attach to running target keeps resetting mcu

跳至解决方案
4,044 次查看
Catosh
Contributor IV

Hi, 

I need to connect to a running target for debugging purposes (s32K11x mcu). 

The debugger resets the MCU event if I select "Connect to running target". 

Hovering with the mouse over the checkbox, the current label appears:  "Currently not supported by SEGGER". 

pastedImage_1.png

But back in the '15s ErichSwas able to connect to a running target without issues (and so was I). 

Is really the connect to running target not supported for segger debugger?

What are suitable probes for this purpose?

Any known workaround?

 

L.

0 项奖励
回复
1 解答
3,762 次查看
Catosh
Contributor IV

Hi Jiri, 

thanks for your reply!  

According to Jlink/Jtrace user guide (soft version 6.40, rev0) there should be the "monitor debugging mode".
This link to segger's wiki provides some hint on that. 

I'm wondering if someone tried successfully it in S32DS for ARM.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,762 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that segger j-link performs reset even when connecting to running target. I tried PE Micro (OpenSDA) - and it can connect to running target without reset. 

Jiri

3,763 次查看
Catosh
Contributor IV

Hi Jiri, 

thanks for your reply!  

According to Jlink/Jtrace user guide (soft version 6.40, rev0) there should be the "monitor debugging mode".
This link to segger's wiki provides some hint on that. 

I'm wondering if someone tried successfully it in S32DS for ARM.

0 项奖励
回复