S32K148 ISR not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 ISR not working

2,321件の閲覧回数
satish_k_singh
Contributor III

Hello ,

I am trying to write an ISR routine  on s32k148 eval board  and would want  that it  detects the switch (PTC 13 on rising edge) and toggle the output  BLUE LED (PORTE 23), but I see the blue LED glowing but the Interrupt is not getting detected when the SW4 is pressed.

So could you please let know if I have missed something.

The below is the sample code.

Config from the  processor expert.

{
.base = PORTC,
.pinPortIdx = 12u,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.passiveFilter = false,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.mux = PORT_MUX_AS_GPIO,
.pinLock = false,
.intConfig = PORT_INT_RISING_EDGE,
.clearIntFlag = true,
.gpioBase = PTC,
.direction = GPIO_INPUT_DIRECTION,
},

{
.base = PORTE,
.pinPortIdx = 23u,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.passiveFilter = false,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.mux = PORT_MUX_AS_GPIO,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = PTE,
.direction = GPIO_OUTPUT_DIRECTION,
},

void FS0B_ISR(void)

{
PINS_DRV_ClearPinIntFlagCmd(PORTC, (1<<13));
PINS_DRV_TogglePins(PTE, (1<<23));

}

main()

{

CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);


PINS_DRV_SetPinDirection(PTC, (1<<13), 0);
PINS_DRV_SetPins(PTE, (1<<23));
INT_SYS_InstallHandler(PORTC_IRQn, FS0B_ISR, (isr_t *)0);
INT_SYS_EnableIRQ(PORTC_IRQn);
PINS_DRV_SetPinIntSel(PORTC,(1<<13),PORT_INT_RISING_EDGE);

}

タグ(4)
0 件の賞賛
返信
1 返信

2,059件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

here is simple example for GPIO Interrupt handler - https://community.nxp.com/docs/DOC-343587 

Hope it helps. 

Jiri