Attach to running target keeps resetting mcu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Attach to running target keeps resetting mcu

ソリューションへジャンプ
4,047件の閲覧回数
Catosh
Contributor IV

Hi, 

I need to connect to a running target for debugging purposes (s32K11x mcu). 

The debugger resets the MCU event if I select "Connect to running target". 

Hovering with the mouse over the checkbox, the current label appears:  "Currently not supported by SEGGER". 

pastedImage_1.png

But back in the '15s ErichSwas able to connect to a running target without issues (and so was I). 

Is really the connect to running target not supported for segger debugger?

What are suitable probes for this purpose?

Any known workaround?

 

L.

0 件の賞賛
返信
1 解決策
3,765件の閲覧回数
Catosh
Contributor IV

Hi Jiri, 

thanks for your reply!  

According to Jlink/Jtrace user guide (soft version 6.40, rev0) there should be the "monitor debugging mode".
This link to segger's wiki provides some hint on that. 

I'm wondering if someone tried successfully it in S32DS for ARM.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,765件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that segger j-link performs reset even when connecting to running target. I tried PE Micro (OpenSDA) - and it can connect to running target without reset. 

Jiri

3,766件の閲覧回数
Catosh
Contributor IV

Hi Jiri, 

thanks for your reply!  

According to Jlink/Jtrace user guide (soft version 6.40, rev0) there should be the "monitor debugging mode".
This link to segger's wiki provides some hint on that. 

I'm wondering if someone tried successfully it in S32DS for ARM.

0 件の賞賛
返信