Adding .elf files to debug context when using multiple binaries?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding .elf files to debug context when using multiple binaries?

Jump to solution
6,717 Views
gearhead1107
Contributor IV

I'm working on a "mini" bootloader which pulls in a bootloader .bin from another project in S32DS. After making the jump to the application, I naturally don't have any source code to step through since it's not part of the project.

I poked around at a few guides, namely this one (“No source available”, or how to Debug Multiple Binaries with GDB and Eclipse | MCU on Eclipse ) and in Debug Configurations-> Startup -> GDB run commands I added the following (where 0x10410 is the .text space according to the map file)
add-symbol-file "[file path]Bootloader_A00.elf" 0x10410

 

In my debugger console I see the following;

add-symbol-file "[file path]Bootloader_A00.elf" 0x10410
add symbol table from file "[file path]Bootloader_A00.elf" at
.text_addr = 0x10410
(y or n) [answered Y; input not from terminal]
Reading symbols from [file path]Bootloader_A00.elf...done.


however after the jump to Bootloader, I still get the "no source available for "_binary_C__Users_[myname]_workspaceS32DS_ARM... at [location in bootloader]" "

I've made sure I'm building in debug, but still can't see my code from the bootloader... any commands that I'm missing here?

1 Solution
5,310 Views
stanish
NXP Employee
NXP Employee

Hello Andrew,

Thanks for your question. I've tested this and I've basically reached the same point.

I'd suggest you to rather switch the symbol files via "Debugger Console" / GDB client console as a workaround.

e.g. to load bootloader symbols type the command below into GDB client console:

symbol-file <Path_to_your_BL_elf>\S32K144_bootloader.elf -readnow

pastedImage_14.png

* refresh the IDE (menu File -> 

pastedImage_13.png

and now the bootloader sources/symbols are available:

pastedImage_20.png

repeat the steps for the application symbol-file:

pastedImage_21.png

In the meantime I'll check with our debugger team what might be wrong with add-symbol-file.

Regards,

Stan

View solution in original post

2 Replies
5,311 Views
stanish
NXP Employee
NXP Employee

Hello Andrew,

Thanks for your question. I've tested this and I've basically reached the same point.

I'd suggest you to rather switch the symbol files via "Debugger Console" / GDB client console as a workaround.

e.g. to load bootloader symbols type the command below into GDB client console:

symbol-file <Path_to_your_BL_elf>\S32K144_bootloader.elf -readnow

pastedImage_14.png

* refresh the IDE (menu File -> 

pastedImage_13.png

and now the bootloader sources/symbols are available:

pastedImage_20.png

repeat the steps for the application symbol-file:

pastedImage_21.png

In the meantime I'll check with our debugger team what might be wrong with add-symbol-file.

Regards,

Stan

5,310 Views
gearhead1107
Contributor IV

Thanks, Stan - this definitely works as a temporary solution.

One important note for anyone following along is that you have to refresh the debug context - not the file explorer context.

0 Kudos
Reply