Activation problem "S32 Design Studio for e200" - need compiler for "Model Based Toolbox 2.0"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Activation problem "S32 Design Studio for e200" - need compiler for "Model Based Toolbox 2.0"

6,470 次查看
kp1991
Contributor II

Hey Guy's,

 

I'm also facing activation problems for S32 PA 1.1.

 

I tried offline and online product activation, but nothing worked for me.

   Offline: "Invalid Offline Response" --->  <ResponseType>CLIENT_CONFIG</ResponseType>

   Online: "Error sending activation request .... (FNP error 50041,41143,34)" (No Firewall, Mobile Network and Company Network)

 

Actually, I only need the s32 e200 compiler for the new "Model Based Library v2.0" for Matlab. Does anybody know a workaround for my problem?

 

Any Updates regarding the new Version - seems like the link is down for a while now...? S32 Design Studio for Power v1.1 - Update 1 available 

 

Regards

Kevin

 

pastedImage_1.png

7 回复数

5,372 次查看
sureshkurukundi
Contributor III

I am facing the problem in installing S32 Design studio in Linux machine (Ubuntu 16.04). When I enter the activation code received in the mail in 'S32DS Activation' dialog box and select the activation type as "online" , I am getting the following error, shown in the screen snippet. Please let me know how to resolve this.
Additionally the desktop is connected to the internet. Thank you.Screenshot from 2018-02-22 19-54-01.png.

0 项奖励
回复

5,372 次查看
stanish
NXP Employee
NXP Employee

Suresh,

I suspect this could be caused by a firewall or an antivirus sw that prevents connection from you computer to the licensing/activation cloud.

I'd recommend you to try use offline activation in this case.

Hope it helps.

Stan

0 项奖励
回复

5,372 次查看
stanish
NXP Employee
NXP Employee

Hello Matthias, Zhongzheng,

First thank you for you reports and apologize about the delay.

Offline activation issue hot fix has been released. Please check the link below.

S32 Design Studio Offline activation issue hot fix 

Hope it helps.

Regards,

Stan

0 项奖励
回复

5,372 次查看
mbu2015
Contributor II

Hello Stan,

everything is fine now.

Thank you!

The next question is posted already :smileywink:

Mit freundlichem Gruss

With Best Regards

Matthias Busch

Embedded Solutions 2.4 (TD-S24)

IAV GmbH

Visitors:

Kauffahrtei 25

09120 CHEMNITZ

GERMANY

Postal:

Auer Straße 54

09366 STOLLBERG

GERMANY

Phone: +49 371 23 7 - 3 46 69

Fax: +49 371 23 7 - 3 41 12

E-Mail: <mailto:[email protected]>

Internet: http://www.iav.de

Sitz/Registered Office: Berlin,

Registergericht/Registration Court: Amtsgericht Charlottenburg,

Registernummer/Company Registration Number: HRB 21 280,

Geschäftsführer/Managing Directors: Kurt Blumenröder, Michael Schubert,

Kai-Stefan Linnenkohl

Vorsitzender des Aufsichtsrates/Chairman of the Supervisory Board: Prof.

Dr. Harald Ludanek

Von: stanish <[email protected]>

An: Matthias Busch <[email protected]>,

Datum: 22.05.2017 22:27

Betreff: Re: - Re: Activation

problem "S32 Design Studio for e200" - need compiler for "Model Based

Toolbox 2.0"

NXP Community

Re: Activation problem "S32 Design Studio for e200" - need compiler for

"Model Based Toolbox 2.0"

reply from Stanislav Sliva in S32 Design Studio - View the full discussion

Hello Matthias, Zhongzheng,

First thank you for you reports and apologize about the delay.

Offline activation issue hot fix has been released. Please check the link

below.

S32 Design Studio Offline activation issue hot fix

Hope it helps.

Regards,

Stan

Reply to this message by replying to this email, or go to the message on

NXP Community

Start a new discussion in S32 Design Studio by email or at NXP Community

Following Re: Activation problem "S32 Design Studio for e200" - need

compiler for "Model Based Toolbox 2.0" in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email

frequency in your email preferences

0 项奖励
回复

5,372 次查看
mbu2015
Contributor II

Hello,

I do have the exact same problem and I think I know why: My companies firewall rules prevent the online registration from succeeding as it worked fine on my private computer which is not limitted in that respect.

So you definitely have to fix the offline activation issue as my guess is that otherwise nearly no-one from the automotive industry will (should) be able to use your stuff!

Regards

Matthias

5,372 次查看
stanish
NXP Employee
NXP Employee

Hello Kevin,

Thanks for your report and we apologize about the inconveniences!

I've checked your activation attempts records and there are offline activation attempts only. Your online registration attempts haven't reached our server. There must be something blocking the communication with our servers. I'll escalate this to the licensing team.

Regarding offline activation issue (Client config response) - we are currently working on a fix. I'm afraid currently there is no workaround.

I'll inform you as soon as there is any update.

Regarding the S32DS power v1.1 update 1 ... this update does not address the issue with offline activation. Anyway I contacted our web team to add this file back into download section - this may take few days.

Thanks for the heads up!

Stan

0 项奖励
回复

5,372 次查看
zhongzhengliu
Contributor I

Hello,

     I have the same question . I tried offline and online product activation, but nothing worked for me. I hope that you can deal with this problem.

    Thank you

pastedImage_1.png

pastedImage_2.png

0 项奖励
回复