ADC and PWM example for MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC and PWM example for MPC5744P

4,590 Views
seize
Contributor III

Is there any example about ADC and PWM for MPC 5744P using S32 design studio?

 

Thanks in advance

 

Hyuntae Choi

Labels (1)
3 Replies

3,805 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

unfortunately, there is not ADC and PWM example for MPC5744P created in S32 Design Studio, but I created ADC example for MPC5775K which you could use.

Please look at the community software example list. There you can find all available examples for MPC56xx and MPC57xx microcontrollers. Examples created directly in S32 Design Studio contain S32DS in their name. All other examples for MPC57xx are created using Green Hills Multi IDE.

https://community.nxp.com/docs/DOC-329623 

If you have any other questions, please feel free to write me back.

Regards,

Martin

3,805 Views
seize
Contributor III

Hi Martin,

Thanks for your kind reply.

Actually, this is my first time using NXP microcontroller and S32 Design

studio, and I have trouble to take first step of using them.

That is why I looking for examples for ADC,PWM and CAN communication, which

are main focus of my project.

I have check the link you provided but there is only three examples for

MPC5744P created in S32 DS.

Can you please recommend anything that help me to understand or to start

MPC5744P and S32 DS?

I already go through reference manual for MPC5744P and user manual for S32

DS.

Best regards,

Hyuntae Choi

2016-12-01 22:36 GMT+09:00 b55689 <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: ADC and PWM example for MPC5744P

reply from Martin Kovar

<https://community.nxp.com/people/b55689?et=watches.email.thread> in *S32

Design Studio* - View the full discussion

<https://community.nxp.com/message/856379?commentID=856379&et=watches.email.thread#comment-856379>

0 Kudos
Reply

3,805 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

about S32 Design Studio, you can check gcc compiler documentation https://gcc.gnu.org/onlinedocs/.  There is also S32 Design Studio community, where you can find usable many information S32 Design Studio .

If you need more information about ADC and PWM, please look at the following document. It is created for MPC5643L, but modules are the same as in MPC5744P.

https://community.nxp.com/docs/DOC-102559 

I think the documents you wrote and the documents above are the main ones you need for successful working with MPC5744P and S32 Design Studio.

If you hit a snag, please feel free to create a question here on community or create NXP support case.

Regards,

Martin