ADC Sample Project Issue S32K344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Sample Project Issue S32K344

1,418件の閲覧回数
Riyasma
Contributor I

Example Project Name: Adc_Sar_Bctu_Ip_example_S32K344

We were using S32K3X4EVB-T172 development board for testing ADC through build in potentiometer and also by interfacing external sensors. The problem we are facing is every time the value continuously changing in the range 600- 1000. Even if I change the analog input value, it keeps on varying in that range only.

please do the needful

Also, if any document is there for example project understanding please provide us.

 

Thanks & Regards

0 件の賞賛
返信
1 返信

1,383件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

can you specify the S32DS and RTD version you are using?
Also describe changes done in demo example, as by default it does not measure voltage on potentiometer (connected to ADC1 S10 channel), but ADC0 bandgap value.

BR, Petr

0 件の賞賛
返信