ADC Sample Project Issue S32K344

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC Sample Project Issue S32K344

912 次查看
Riyasma
Contributor I

Example Project Name: Adc_Sar_Bctu_Ip_example_S32K344

We were using S32K3X4EVB-T172 development board for testing ADC through build in potentiometer and also by interfacing external sensors. The problem we are facing is every time the value continuously changing in the range 600- 1000. Even if I change the analog input value, it keeps on varying in that range only.

please do the needful

Also, if any document is there for example project understanding please provide us.

 

Thanks & Regards

0 项奖励
回复
1 回复

877 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

can you specify the S32DS and RTD version you are using?
Also describe changes done in demo example, as by default it does not measure voltage on potentiometer (connected to ADC1 S10 channel), but ADC0 bandgap value.

BR, Petr

0 项奖励
回复