For S32 Design Studio v3.5 and earlier, there is a known issue when the S32 Configuration Tools are invoked from command line from a location outside of the S32DS installation directory.
The following error is reported:
java.lang.reflect.InvocationTargetException
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method)
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance(Unknown Source)
at java.base/jdk.internal.reflect.DelegatingConstructorAccessorImpl.newInstance(Unknown Source)
at java.base/java.lang.reflect.Constructor.newInstance(Unknown Source)
at com.nxp.swtools.common.utils.runtime.SingletonProvider.getSingletonInstance(SingletonProvider.java:46)
at com.nxp.swtools.common.ui.utils.swt.internal.SWTFactory.getSingletonInstance(SWTFactory.java:421)
at com.nxp.swtools.common.ui.utils.swt.SWTFactoryProxy.getSingletonInstance(SWTFactoryProxy.java:448)
at com.nxp.swtools.dcd.controller.DCDController.getInstance(DCDController.java:84)
at com.nxp.swtools.dcd.DCDStartup.earlyStartup(DCDStartup.java:23)
at com.nxp.swtools.provider.SWToolsPlatform.initializeAllTools(SWToolsPlatform.java:702)
at com.nxp.swtools.framework.Application.start(Application.java:475)
at com.nxp.swtools.framework.Application.start(Application.java:445)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.base/java.lang.reflect.Method.invoke(Unknown Source)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:654)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:591)
at org.eclipse.equinox.launcher.Main.run(Main.java:1462)
Caused by: java.lang.NoClassDefFoundError: javafx/beans/property/SimpleBooleanProperty
at com.nxp.swtools.bootimage.controller.ABootController.<init>(ABootController.java:37)
at com.nxp.swtools.dcd.dcf.common.DCDCommonController.<init>(DCDCommonController.java:90)
at com.nxp.swtools.dcd.controller.DCDController.<init>(DCDController.java:43)
... 24 more
Caused by: java.lang.ClassNotFoundException: javafx.beans.property.SimpleBooleanProperty cannot be found by com.nxp.swtools.bootimage_1.0.0.202207251223
at org.eclipse.osgi.internal.loader.BundleLoader.findClass(BundleLoader.java:519)
at org.eclipse.osgi.internal.loader.ModuleClassLoader.loadClass(ModuleClassLoader.java:170)
at java.base/java.lang.ClassLoader.loadClass(Unknown Source)
Resolution:
To resolve the issue:
- Invoke the command from within the installation directory, for example, from 'C:\NXP\S32DS.3.5\eclipse'
OR
-
Change "{S32DS Installation Folder}\eclipse\s32ds.ini" by setting the javafx path from relative to absolute. So, if default installation is used, then:
Change
-Defxclipse.java-modules.dir=jre/javafx-sdk-11.0.2/lib
To
-Defxclipse.java-modules.dir=C:/NXP/S32DS.3.5/eclipse/jre/javafx-sdk-11.0.2/lib
In addition, if it is desired to suppress unimportant warning messages:
go to {S32DS installation folder}\eclipse\configuration, open logging.properties file and change com.nxp.swtools.level = SEVERE