| 
 | 
 | 
 | 
| Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 2 | 
 | |
| 
 | 
 | 
 | 
• S32DS-3506 - [e200][MPC5744P] unable to connect to secured device - addressed by adding unsecure support for MPC5744P devices
• S32DS-7326 - [e200][MPC5634M] Exception occurs when accessing peripheral A registers - MMU init script error is resolved by updating the script
• S32DS-7991 - [e200 2017.R1] Semihosting disabling interrupts is resolved by not disabling interrupts when stepping over specific instruction
• S32DS-7177 - [MPC5634M] unable to access RAM in the debug session
• S32DS-7896 - [e200] default linker sections (.got2, .jsr...) are missing in the linker script file
• S32DS-3681 - [S32DS E200 B170421] Project build fail with Library support = newlib, the startup.S update to add section _fini
The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link)
 
Select all available items and click "Next" button.
This will starts the update installation process.
Added tags for resolved issues in this update.
GCC:
CMPE200GCC-168
cmpe200gcc-181
cmpe200gcc-183
CMPE200GCC-184
Binutils:
CMPE200GCC-176
Newlib:
cmpe200gcc-126
cmpe200gcc-178
CMPE200GCC-170