HOWTO: Reset MCU in S32 Design Studio debugger (Pemicro/OpenSDA interface)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HOWTO: Reset MCU in S32 Design Studio debugger (Pemicro/OpenSDA interface)

HOWTO: Reset MCU in S32 Design Studio debugger (Pemicro/OpenSDA interface)

The ability to reset target MCU via debugger (also known as "in-target reset") is one of the essential feature when it comes to e.g. debugging of a code that is getting into an Exception/Fault Handler or situations like "...why my code works fine in the debugger, but fails without debug..."

S32 Design Studio offers this feature for all Pemicro debug interfaces (Multilink Universal/FX, OpenSDA) and it is available in all S32 Design studio flavors (S32DS ARM, S32DS Power, S32DS Vision)

Reset button icon is active only in the active debug session (debug perspective) and in the root debug context only. 

By default the reset icon is inactive during project debugging:

pastedImage_8.png

To activate the reset icon change the Debug view context to the root one.

pastedImage_2.png

After reset is completed the execution stops at the application reset vector and the information about reset that has just occurred is displayed in GDB server console.

pastedImage_9.png

It is also possible to execute initialization script (.mac) which is triggered by the reset action. The reset script can be selected in the  Debug Configuration (Debugger Tab -> Advanced Options -> Enable Initialization Script)

pastedImage_1.png

For more information about initialization scripting capabilities please contact www.pemicro.com

ラベル(1)
コメント

Is there any command that can do this in a debugger console.

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎01-04-2018 02:53 AM
更新者: