HOWTO: Create a Blinking LED application project for S32R45 using S32 RTD Non AUTOSAR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HOWTO: Create a Blinking LED application project for S32R45 using S32 RTD Non AUTOSAR

HOWTO: Create a Blinking LED application project for S32R45 using S32 RTD Non AUTOSAR

This document shows the step-by-step process to create a simple blinking LED application for the S32R45 device using the S32 RTD non-AUTOSAR drivers. For this example used for the S32R45 EVB, connected via ethernet connection through S32 Debugger.

Preparation

  1. Setup the software tools
    1. Install S32 Design Studio for S32 Platform
    2. Install the S32R45 development package and the S32R45 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools.
      image.pngimage.png
  2. Launch S32 Design Studio for S32 Platform

Procedure

  1. New S32DS Project
    image.pngimage.png
    OR
    image.pngimage.png
  2. Provide a name for the project, for example 'Blinking_LED_RTD_No_AUTOSAR'. The name must be entered with no space characters.
  3. Expand Family S32R45, Select S32R45 Cortex-M7image.pngimage.png
  4. Click Next
  5. And Click '…' button next to SDKs
    DanielBarbu_0-1718878497273.pngDanielBarbu_0-1718878497273.png

     

  6. Check box next to PlatformSDK_S32RXX_4_0_0_S32R45_M7_0. (or whichever latest SDK for the S32R45 is installed). Click OK
    image.pngimage.png
  7. Now, uncheck the selection mark for other core, i.e. for Cortex-M7-1 , Cortex-M7-2
    DanielBarbu_1-1718878543486.pngDanielBarbu_1-1718878543486.png

     

  8. Click Finish. Wait for project generation wizard to complete, then expand the project within the Project Explorer view to show the contents.
    image.pngimage.png
  9. To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way by double-click on the MEX file.
    image.pngimage.png
  10. By default, the Pins tool is then presented. For the Blinking LED example, one pin must be configured as output. The S32R45 EVB has an user LED connected pin is PD_05.

    From the Peripheral Signals tab left to the Pins tool perspective layout, locate Open the Siul2_0 from the peripheral signals tab. And from the drop down menu select “gpio,53 PD_05” option as per shown in the following image.

    We are using PD_05 for the GPIO usage, so we are routing SIUL2_0 GPIO signal to this pin.
    image.pngimage.png
    Select gpio53 -> PD_05 as shown below :
    image.pngimage.png
  11. The Direction required! menu will appear. Select Output then OK.
    image.pngimage.png
  12. In Routing Details view, notice a new line has been added and highlighted in yellow.
    image.pngimage.png
  13. Add ‘LED’ to the Label and Identifier columns for the PORTD 5 pin.
    image.pngimage.png
  14. Code Preview
    image.pngimage.pngimage.pngimage.png
  15. Go to Peripherals tool and add Siul2_Dio to enable LED blinking, it adjacent to the user LED on S32R45 EVB.
    1. Click on the Peripherals Tool icon from the Eclipse Perspective navigation bar.
      image.pngimage.png
    2. From the Components view, click on ‘Add a new configuration component…’ button from the Drivers category. This will bring up a list of all configuration components.
      image.pngimage.png
    3. Locate and then select the ‘Siul2_Dio’ component from the list and click OK. Do not worry about the warning message. It is only indicating that the driver is not already part of the current project. The associated driver package will be added automatically. Note: It may be necessary to change the selection at the top from ‘Present in the tool-chain project’ to ‘All’.

      The DIO driver provides services for reading and writing to/from DIO Channels.
      image.pngimage.png
  16. The Gpio_Dio driver requires no further configuration. Click Save to store all changes to the .MEX file.
    image.pngimage.png
  17. Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar.
    image.pngimage.png
  18. To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective.
    image.pngimage.png
  19. If not already open, in the project window click the ‘>’ next to the ‘src’ folder to show the contents, then double click ‘main.c’ file to open it. This is where the application code will be added.
    image.pngimage.png
  20. Before the pin can be controlled, it needs to be initialized using the configuration information that was generated from the S32 Configuration tools. Initialize all pins using the Port driver by adding the following line: Insert the following line into main, after the comment 'Write your code here':

    /* Initialize all pins using the Port driver */
    Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
    image.pngimage.png

  21. Now, add logic for the LED turn and off. To turn the pin on and off with some delays in-between to cause the LED to blink. Make the delays long enough to be perceptible.
    1. Add line to initialize variable
      uint8 i = 0;
    2. Change the code within the provided for loop, and add the following lines:


      //logic for blinking LED 10 times
      while (i++ < 10)
      {
             Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 1U);
             TestDelay(4000000);
             Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 0U);
             TestDelay(4000000);
      }
      image.pngimage.png

  22. Before the 'main' function, add a delay function as follows:

    void TestDelay(uint32 delay);
    void TestDelay(uint32 delay)
    {
       static volatile uint32 DelayTimer = 0;
       while (DelayTimer<delay)
       {
           DelayTimer++;
       }
       DelayTimer=0;
    }
    image.pngimage.png

  23. Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application:

    Remove
    #include "Mcal.h"

    Add

    #include "Siul2_Port_Ip.h"
    #include "Siul2_Dio_Ip.h"
    image.pngimage.png

  24. Build 'Blinking_LED_RTD_No_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'.
    image.pngimage.png
  25. After the build completes, check that there are no errors.
    image.pngimage.png
  26. Open Debug Configurations and select 'Blinking_LED_RTD_No_AUTOSAR_Debug_RAM'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist.
    image.pngimage.png
  27. Now, you need to Select the Interface (Ethernet or USB) by which the S32 Debug Probe is connected.
    image.pngimage.png
    1. If connected via USB and this option is selected for interface, then the COM port will be detected automatically (in the rare event where 2 or more S32 Debug Probes are connected via USB to the host PC, then it may be necessary to select which COM port is correct for the probe which is connected to the EVB)
      image.pngimage.png
    2. If connected via Ethernet, enter the IP address of the probe. See the S32 Debug Probe User Manual for ways to determine the IP address.
      image.pngimage.png
  28. Click Debug
  29. To see the LED blink, click ‘Resume'.
    image.pngimage.png
  30. This code as it will blink the LED 10 times, you can make changes in for loop condition to blink it infinitely.
%3CLINGO-SUB%20id%3D%22lingo-sub-1563699%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E5%A6%82%E4%BD%95%EF%BC%9A%E4%BD%BF%E7%94%A8%20S32%20RTD%20Non%20AUTOSAR%20%E4%B8%BA%20S32R45%20%E5%88%9B%E5%BB%BA%E9%97%AA%E7%83%81%20LED%20%E5%BA%94%E7%94%A8%E9%A1%B9%E7%9B%AE%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1563699%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%0A%3CP%3E%E6%9C%AC%E6%96%87%E6%A1%A3%E5%B1%95%E7%A4%BA%E4%BA%86%E4%BD%BF%E7%94%A8%20S32%20RTD%20%E9%9D%9E%20AUTOSAR%20%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E4%B8%BA%20S32R45%20%E8%AE%BE%E5%A4%87%E5%88%9B%E5%BB%BA%E7%AE%80%E5%8D%95%E9%97%AA%E7%83%81%20LED%20%E5%BA%94%E7%94%A8%E7%A8%8B%E5%BA%8F%E7%9A%84%E5%88%86%E6%AD%A5%E8%BF%87%E7%A8%8B%E3%80%82%E6%AD%A4%E7%A4%BA%E4%BE%8B%E7%94%A8%E4%BA%8E%20S32R45%20EVB%EF%BC%8C%E9%80%9A%E8%BF%87%20S32%20%E8%B0%83%E8%AF%95%E5%99%A8%E9%80%9A%E8%BF%87%E4%BB%A5%E5%A4%AA%E7%BD%91%E8%BF%9E%E6%8E%A5%E8%BF%9B%E8%A1%8C%E8%BF%9E%E6%8E%A5%E3%80%82%3C%2FP%3E%0A%3CH1%20id%3D%22toc-hId-500638132%22%20id%3D%22toc-hId-1304007932%22%3E%3CSTRONG%3E%3CU%3E%E5%87%86%E5%A4%87%E5%B7%A5%E4%BD%9C%3C%2FU%3E%3C%2FSTRONG%3E%3C%2FH1%3E%0A%3COL%3E%0A%3CLI%3E%E8%AE%BE%E7%BD%AE%E8%BD%AF%E4%BB%B6%E5%B7%A5%E5%85%B7%0A%3COL%20class%3D%22lia-list-style-type-lower-alpha%22%3E%0A%3CLI%3E%E5%AE%89%E8%A3%85%20S32%20Design%20Studio%20for%20S32%20Platform%3C%2FLI%3E%0A%3CLI%3E%E5%AE%89%E8%A3%85%20S32R45%20%E5%BC%80%E5%8F%91%E5%8C%85%E5%92%8C%20S32R45%20RTD%20AUTOSAR%204.4%E3%80%82S32%20%E9%85%8D%E7%BD%AE%E5%B7%A5%E5%85%B7%E9%83%BD%E9%9C%80%E8%A6%81%E8%BF%99%E4%B8%A4%E8%80%85%E3%80%82%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20502px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20502px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202672i40FC2949FFC6E40F%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3C%2FOL%3E%0A%3C%2FLI%3E%0A%3CLI%3E%E5%90%AF%E5%8A%A8%20S32%20Design%20Studio%20for%20S32%20Platform%3C%2FLI%3E%0A%3C%2FOL%3E%0A%3CH1%20id%3D%22toc-hId--1306816331%22%20id%3D%22toc-hId--503446531%22%3E%3CSTRONG%3E%3CU%3E%E6%B5%81%E7%A8%8B%3C%2FU%3E%3C%2FSTRONG%3E%3C%2FH1%3E%0A%3COL%3E%0A%3CLI%3E%E6%96%B0%E7%9A%84%20S32DS%20%E9%A1%B9%E7%9B%AE%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20685px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20685px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202674i50B5668E1E1F39A7%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%E6%88%96%E8%80%85%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20424px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20424px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202675i7CE05F1A7EABA1E8%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E4%B8%BA%E9%A1%B9%E7%9B%AE%E6%8F%90%E4%BE%9B%E4%B8%80%E4%B8%AA%E5%90%8D%E7%A7%B0%EF%BC%8C%E4%BE%8B%E5%A6%82%E2%80%9CBlinking_LED_RTD_No_AUTOSAR%E2%80%9D%E3%80%82%E8%BE%93%E5%85%A5%E7%9A%84%E5%90%8D%E7%A7%B0%E4%B8%8D%E5%BE%97%E5%8C%85%E5%90%AB%E7%A9%BA%E6%A0%BC%E3%80%82%3C%2FLI%3E%0A%3CLI%3E%E6%89%A9%E5%B1%95%20S32R45%20%E7%B3%BB%E5%88%97%EF%BC%8C%E9%80%89%E6%8B%A9%20S32R45%20Cortex-M7%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20642px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20642px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202676i2C6D2C67E8214C05%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E5%8D%95%E5%87%BB%3CSTRONG%3E%E2%80%9C%E4%B8%8B%E4%B8%80%E6%AD%A5%E2%80%9D%3C%2FSTRONG%3E%3C%2FLI%3E%0A%3CLI%3E%E7%84%B6%E5%90%8E%E7%82%B9%E5%87%BB%20SDKs%20%E6%97%81%E8%BE%B9%E7%9A%84%E2%80%9C%E2%80%A6%E2%80%9D%E6%8C%89%E9%92%AE%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22DanielBarbu_0-1718878497273.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22DanielBarbu_0-1718878497273.png%22%20style%3D%22width%3A%20774px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F285053i8E086411299E3AED%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22DanielBarbu_0-1718878497273.png%22%20alt%3D%22DanielBarbu_0-1718878497273.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EDanielBarbu_0-1718878497273.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%0A%20%3CBR%20%2F%3E%0A%3C%2FLI%3E%0A%3CLI%3E%E9%80%89%E4%B8%AD%20PlatformSDK_S32RXX_4_0_0_S32R45_M7_0%20%E6%97%81%E8%BE%B9%E7%9A%84%E5%A4%8D%E9%80%89%E6%A1%86%E3%80%82%EF%BC%88%E6%88%96%E5%AE%89%E8%A3%85%E4%BA%86%E9%80%82%E7%94%A8%E4%BA%8E%20S32R45%20%E7%9A%84%E4%BB%BB%E4%BD%95%E6%9C%80%E6%96%B0%20SDK%EF%BC%89%E3%80%82%E5%8D%95%E5%87%BB%3CSTRONG%3E%E2%80%9C%E7%A1%AE%E5%AE%9A%E2%80%9D%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202679i3F908D52FF2AD54D%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSTRONG%3E%3C%2FLI%3E%0A%3CLI%3E%E7%8E%B0%E5%9C%A8%EF%BC%8C%E5%8F%96%E6%B6%88%E9%80%89%E4%B8%AD%E5%85%B6%E4%BB%96%E6%A0%B8%E5%BF%83%E7%9A%84%E9%80%89%E6%8B%A9%E6%A0%87%E8%AE%B0%EF%BC%8C%E5%8D%B3%20Cortex-M7-1%E3%80%81Cortex-M7-2%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22DanielBarbu_1-1718878543486.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22DanielBarbu_1-1718878543486.png%22%20style%3D%22width%3A%20773px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F285054i138F407F0334636C%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22DanielBarbu_1-1718878543486.png%22%20alt%3D%22DanielBarbu_1-1718878543486.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EDanielBarbu_1-1718878543486.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%0A%20%3CBR%20%2F%3E%0A%3C%2FLI%3E%0A%3CLI%3E%E7%82%B9%E5%87%BB%20%E2%80%9CFinish%E2%80%9D%E3%80%82%E7%AD%89%E5%BE%85%E9%A1%B9%E7%9B%AE%E7%94%9F%E6%88%90%E5%90%91%E5%AF%BC%E5%AE%8C%E6%88%90%EF%BC%8C%E7%84%B6%E5%90%8E%E5%9C%A8%E9%A1%B9%E7%9B%AE%E8%B5%84%E6%BA%90%E7%AE%A1%E7%90%86%E5%99%A8%E8%A7%86%E5%9B%BE%E4%B8%AD%E5%B1%95%E5%BC%80%E9%A1%B9%E7%9B%AE%E4%BB%A5%E6%98%BE%E7%A4%BA%E5%86%85%E5%AE%B9%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20327px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20327px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202692iC301A06427EA9C27%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E8%A6%81%E6%8E%A7%E5%88%B6%E6%9D%BF%E4%B8%8A%E7%9A%84%20LED%EF%BC%8C%E9%9C%80%E8%A6%81%E5%9C%A8%20Pins%20Tool%20%E4%B8%AD%E8%BF%9B%E8%A1%8C%E4%B8%80%E4%BA%9B%E9%85%8D%E7%BD%AE%E3%80%82%E6%9C%89%E5%A4%9A%E7%A7%8D%E6%96%B9%E6%B3%95%E5%8F%AF%E4%BB%A5%E5%AE%9E%E7%8E%B0%E8%BF%99%E4%B8%80%E7%82%B9%EF%BC%8C%E5%85%B6%E4%B8%AD%E4%B8%80%E7%A7%8D%E7%AE%80%E5%8D%95%E7%9A%84%E6%96%B9%E6%B3%95%E6%98%AF%E5%8F%8C%E5%87%BB%20MEX%20%E6%96%87%E4%BB%B6%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202693i9CCD44523572AB67%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E9%BB%98%E8%AE%A4%E6%83%85%E5%86%B5%E4%B8%8B%EF%BC%8C%E4%BC%9A%E6%98%BE%E7%A4%BA%20Pins%20%E5%B7%A5%E5%85%B7%E3%80%82%E5%AF%B9%E4%BA%8E%E9%97%AA%E7%83%81%20LED%20%E7%A4%BA%E4%BE%8B%EF%BC%8C%E5%BF%85%E9%A1%BB%E5%B0%86%E4%B8%80%E4%B8%AA%E5%BC%95%E8%84%9A%E9%85%8D%E7%BD%AE%E4%B8%BA%E8%BE%93%E5%87%BA%E3%80%82S32R45%20EVB%20%E6%9C%89%E4%B8%80%E4%B8%AA%E7%94%A8%E6%88%B7%20LED%20%E8%BF%9E%E6%8E%A5%E5%BC%95%E8%84%9A%E6%98%AF%20PD_05%E3%80%82%3CBR%20%2F%3E%3CBR%20%2F%3E%E4%BB%8E%E2%80%9C%E5%A4%96%E8%AE%BE%E4%BF%A1%E5%8F%B7%E2%80%9D%E9%80%89%E9%A1%B9%E5%8D%A1%E5%B7%A6%E4%BE%A7%E7%9A%84%E2%80%9C%E5%BC%95%E8%84%9A%E2%80%9D%E5%B7%A5%E5%85%B7%E9%80%8F%E8%A7%86%E5%B8%83%E5%B1%80%E4%B8%AD%EF%BC%8C%E6%89%BE%E5%88%B0%E2%80%9C%E4%BB%8E%E5%A4%96%E8%AE%BE%E4%BF%A1%E5%8F%B7%E2%80%9D%E9%80%89%E9%A1%B9%E5%8D%A1%E6%89%93%E5%BC%80%20Siul2_0%E3%80%82%E5%B9%B6%E4%BB%8E%E4%B8%8B%E6%8B%89%E8%8F%9C%E5%8D%95%E4%B8%AD%E9%80%89%E6%8B%A9%E2%80%9Cgpio%2C53%20PD_05%E2%80%9D%E9%80%89%E9%A1%B9%EF%BC%8C%E5%A6%82%E4%B8%8B%E5%9B%BE%E6%89%80%E7%A4%BA%E3%80%82%3CBR%20%2F%3E%3CBR%20%2F%3E%E6%88%91%E4%BB%AC%E4%BD%BF%E7%94%A8%20PD_05%20%E4%BD%9C%E4%B8%BA%20GPIO%EF%BC%8C%E5%9B%A0%E6%AD%A4%E6%88%91%E4%BB%AC%E5%B0%86%20SIUL2_0%20GPIO%20%E4%BF%A1%E5%8F%B7%E8%B7%AF%E7%94%B1%E5%88%B0%E6%AD%A4%E5%BC%95%E8%84%9A%E3%80%82%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20200px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202696i2B4DDC10AB6613F8%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%E9%80%89%E6%8B%A9gpio53-%26gt%3BPD_05%EF%BC%8C%E5%A6%82%E4%B8%8B%E6%89%80%E7%A4%BA%EF%BC%9A%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20313px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202698iD62E8E41CEA9304D%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E9%9C%80%E8%A6%81%E6%96%B9%E5%90%91%EF%BC%81%E5%B0%86%E4%BC%9A%E5%87%BA%E7%8E%B0%E8%8F%9C%E5%8D%95%E3%80%82%E9%80%89%E6%8B%A9%E2%80%9C%E8%BE%93%E5%87%BA%E2%80%9D%EF%BC%8C%E7%84%B6%E5%90%8E%E9%80%89%E6%8B%A9%E2%80%9C%E7%A1%AE%E5%AE%9A%E2%80%9D%E3%80%82%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202701iB9DC1F0337C565D8%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E5%9C%A8%E2%80%9CRouting%20Details%E2%80%9D%E8%A7%86%E5%9B%BE%E4%B8%AD%EF%BC%8C%E8%AF%B7%E6%B3%A8%E6%84%8F%E5%B7%B2%E6%B7%BB%E5%8A%A0%E4%B8%80%E6%9D%A1%E6%96%B0%E8%A1%8C%E5%B9%B6%E4%BB%A5%E9%BB%84%E8%89%B2%E7%AA%81%E5%87%BA%E6%98%BE%E7%A4%BA%E3%80%82%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202703i0CA5FEBA19CD6146%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E5%B0%86%E2%80%9CLED%E2%80%9D%E6%B7%BB%E5%8A%A0%E5%88%B0%20PORTD%205%20%E5%BC%95%E8%84%9A%E7%9A%84%E6%A0%87%E7%AD%BE%E5%92%8C%E6%A0%87%E8%AF%86%E7%AC%A6%E5%88%97%E3%80%82%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202705i6FF5B95B7DAD1128%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E4%BB%A3%E7%A0%81%E9%A2%84%E8%A7%88%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20855px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20855px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202707iB0AE9E5B54FCB20C%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20771px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20771px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202711iB4A20197F3E69FBF%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E8%BD%AC%E5%88%B0%E5%A4%96%E8%AE%BE%E5%B7%A5%E5%85%B7%E5%B9%B6%E6%B7%BB%E5%8A%A0%20Siul2_Dio%20%E4%BB%A5%E5%90%AF%E7%94%A8%20LED%20%E9%97%AA%E7%83%81%EF%BC%8C%E5%AE%83%E4%B8%8E%20S32R45%20EVB%20%E4%B8%8A%E7%9A%84%E7%94%A8%E6%88%B7%20LED%20%E7%9B%B8%E9%82%BB%E3%80%82%0A%3COL%20class%3D%22lia-list-style-type-lower-alpha%22%3E%0A%3CLI%3E%E5%8D%95%E5%87%BB%20Eclipse%20Perspective%20%E5%AF%BC%E8%88%AA%E6%A0%8F%E4%B8%AD%E7%9A%84%E2%80%9C%E5%A4%96%E8%AE%BE%E5%B7%A5%E5%85%B7%E2%80%9D%E5%9B%BE%E6%A0%87%E3%80%82%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20530px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20530px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202712i7D1A3640EE5AE002%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E5%9C%A8%E7%BB%84%E4%BB%B6%E8%A7%86%E5%9B%BE%E4%B8%AD%EF%BC%8C%E5%8D%95%E5%87%BB%3CSTRONG%3E%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%3C%2FSTRONG%3E%E7%B1%BB%E5%88%AB%E4%B8%AD%E7%9A%84%E2%80%9C%E6%B7%BB%E5%8A%A0%E6%96%B0%E9%85%8D%E7%BD%AE%E7%BB%84%E4%BB%B6...%E2%80%9D%E6%8C%89%E9%92%AE%E3%80%82%E8%BF%99%E5%B0%86%E6%98%BE%E7%A4%BA%E6%89%80%E6%9C%89%E9%85%8D%E7%BD%AE%E7%BB%84%E4%BB%B6%E7%9A%84%E5%88%97%E8%A1%A8%E3%80%82%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20563px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20563px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202713iF45092ADF98BED46%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E4%BB%8E%E5%88%97%E8%A1%A8%E4%B8%AD%E6%89%BE%E5%88%B0%E5%B9%B6%E9%80%89%E6%8B%A9%E2%80%9CSiul2_Dio%E2%80%9D%E7%BB%84%E4%BB%B6%EF%BC%8C%E7%84%B6%E5%90%8E%E5%8D%95%E5%87%BB%E2%80%9C%E7%A1%AE%E5%AE%9A%E2%80%9D%E3%80%82%E4%B8%8D%E8%A6%81%E6%8B%85%E5%BF%83%E8%AD%A6%E5%91%8A%E4%BF%A1%E6%81%AF%E3%80%82%E8%BF%99%E4%BB%85%E8%A1%A8%E6%98%8E%E8%AF%A5%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E8%BF%98%E4%B8%8D%E6%98%AF%E5%BD%93%E5%89%8D%E9%A1%B9%E7%9B%AE%E7%9A%84%E4%B8%80%E9%83%A8%E5%88%86%E3%80%82%E7%9B%B8%E5%85%B3%E7%9A%84%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E5%8C%85%E5%B0%86%E8%A2%AB%E8%87%AA%E5%8A%A8%E6%B7%BB%E5%8A%A0%E3%80%82%E6%B3%A8%E6%84%8F%EF%BC%9A%E5%8F%AF%E8%83%BD%E9%9C%80%E8%A6%81%E5%B0%86%E9%A1%B6%E9%83%A8%E7%9A%84%E9%80%89%E6%8B%A9%E4%BB%8E%E2%80%9C%E5%B7%A5%E5%85%B7%E9%93%BE%E9%A1%B9%E7%9B%AE%E4%B8%AD%E7%9A%84%E5%91%88%E7%8E%B0%E2%80%9D%E6%9B%B4%E6%94%B9%E4%B8%BA%E2%80%9C%E5%85%A8%E9%83%A8%E2%80%9D%E3%80%82%3CBR%20%2F%3E%3CBR%20%2F%3EDIO%20%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E6%8F%90%E4%BE%9B%E5%AF%B9%20DIO%20%E9%80%9A%E9%81%93%E8%BF%9B%E8%A1%8C%E8%AF%BB%E5%86%99%E7%9A%84%E6%9C%8D%E5%8A%A1%E3%80%82%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20629px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20629px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202714i4D09A0B5F885BE29%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3C%2FOL%3E%0A%3C%2FLI%3E%0A%3CLI%3EGpio_Dio%20%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E4%B8%8D%E9%9C%80%E8%A6%81%E8%BF%9B%E4%B8%80%E6%AD%A5%E9%85%8D%E7%BD%AE%E3%80%82%E7%82%B9%E5%87%BB%3CSTRONG%3E%E4%BF%9D%E5%AD%98%3C%2FSTRONG%3E%E4%BB%A5%E5%B0%86%E6%89%80%E6%9C%89%E6%9B%B4%E6%94%B9%E4%BF%9D%E5%AD%98%E5%88%B0.MEX%E6%96%87%E4%BB%B6%E4%B8%AD%E3%80%82%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20734px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20734px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202715iCF6C1A7BA0BA7FFA%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E7%8E%B0%E5%9C%A8%EF%BC%8C%E8%AE%BE%E5%A4%87%E9%85%8D%E7%BD%AE%E5%B7%B2%E5%AE%8C%E6%88%90%EF%BC%8C%E5%8F%AF%E4%BB%A5%E7%94%9F%E6%88%90%20RTD%20%E9%85%8D%E7%BD%AE%E4%BB%A3%E7%A0%81%E3%80%82%E4%BB%8E%E8%8F%9C%E5%8D%95%E6%A0%8F%E4%B8%AD%E7%82%B9%E5%87%BB%20%E2%80%9CUpdate%20Code%E2%80%9D%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20911px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20911px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202716i4965A987356F42E0%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E8%A6%81%E6%8E%A7%E5%88%B6%E5%88%9A%E5%88%9A%E9%85%8D%E7%BD%AE%E7%9A%84%E8%BE%93%E5%87%BA%E5%BC%95%E8%84%9A%EF%BC%8C%E9%9C%80%E8%A6%81%E7%BC%96%E5%86%99%E4%B8%80%E4%BA%9B%E5%BA%94%E7%94%A8%E4%BB%A3%E7%A0%81%E3%80%82%E8%BF%94%E5%9B%9E%20%E2%80%9CC%2FC%2B%2B%E2%80%9D%20%E9%80%8F%E8%A7%86%E5%9B%BE%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20514px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20514px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202717i0C595F719D331429%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E5%A6%82%E6%9E%9C%E5%B0%9A%E6%9C%AA%E6%89%93%E5%BC%80%EF%BC%8C%E5%9C%A8%E9%A1%B9%E7%9B%AE%E7%AA%97%E5%8F%A3%E4%B8%AD%E7%82%B9%E5%87%BB%20%E2%80%9Csrc%E2%80%9D%20%E6%96%87%E4%BB%B6%E5%A4%B9%E6%97%81%E8%BE%B9%E7%9A%84%20%E2%80%9C%26gt%3B%E2%80%9D%20%E4%BB%A5%E6%98%BE%E7%A4%BA%E5%86%85%E5%AE%B9%EF%BC%8C%E7%84%B6%E5%90%8E%E5%8F%8C%E5%87%BB%20%E2%80%9Cmain.c%E2%80%9D%20%E6%96%87%E4%BB%B6%E5%B0%86%E5%85%B6%E6%89%93%E5%BC%80%E3%80%82%E5%BA%94%E7%94%A8%E4%BB%A3%E7%A0%81%E5%B0%86%E6%B7%BB%E5%8A%A0%E5%88%B0%E6%AD%A4%E5%A4%84%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20553px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20553px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202718i5445B41501E13ED4%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E5%9C%A8%E6%8E%A7%E5%88%B6%E5%BC%95%E8%84%9A%E4%B9%8B%E5%89%8D%EF%BC%8C%E9%9C%80%E8%A6%81%E4%BD%BF%E7%94%A8%E4%BB%8E%20S32%20%E9%85%8D%E7%BD%AE%E5%B7%A5%E5%85%B7%E7%94%9F%E6%88%90%E7%9A%84%E9%85%8D%E7%BD%AE%E4%BF%A1%E6%81%AF%E8%BF%9B%E8%A1%8C%E5%88%9D%E5%A7%8B%E5%8C%96%E3%80%82%E9%80%9A%E8%BF%87%E6%B7%BB%E5%8A%A0%E4%BB%A5%E4%B8%8B%E8%A1%8C%EF%BC%8C%E4%BD%BF%E7%94%A8%E7%AB%AF%E5%8F%A3%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E5%88%9D%E5%A7%8B%E5%8C%96%E6%89%80%E6%9C%89%E5%BC%95%E8%84%9A%EF%BC%9A%E5%B0%86%E4%BB%A5%E4%B8%8B%E8%A1%8C%E6%8F%92%E5%85%A5%E5%88%B0%E4%B8%BB%E7%A8%8B%E5%BA%8F%E4%B8%AD%EF%BC%8C%E5%9C%A8%E6%B3%A8%E9%87%8A%E2%80%9C%E5%9C%A8%E6%AD%A4%E5%A4%84%E7%BC%96%E5%86%99%E4%BB%A3%E7%A0%81%E2%80%9D%E4%B9%8B%E5%90%8E%EF%BC%9A%3CBR%20%2F%3E%3CBR%20%2F%3E%0A%3CP%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%20color%3D%22%23008000%22%3E%2F*%20%E4%BD%BF%E7%94%A8%E7%AB%AF%E5%8F%A3%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E5%88%9D%E5%A7%8B%E5%8C%96%E6%89%80%E6%9C%89%E5%BC%95%E8%84%9A%20*%2F%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CSPAN%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3ESiul2_Port_Ip_Init%EF%BC%88%E5%B7%B2%E9%85%8D%E7%BD%AE%E5%BC%95%E8%84%9A%E6%95%B0%E9%87%8F0%EF%BC%8Cg_pin_mux_InitConfigArr0%EF%BC%89%EF%BC%9B%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20727px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20727px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202719i8CC863B91D25FB67%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3C%2FLI%3E%0A%3CLI%3E%3CSPAN%3E%E7%8E%B0%E5%9C%A8%EF%BC%8C%E6%B7%BB%E5%8A%A0%20LED%20%E7%82%B9%E4%BA%AE%E5%92%8C%E7%86%84%E7%81%AD%E7%9A%84%E9%80%BB%E8%BE%91%E3%80%82%E9%80%9A%E8%BF%87%E5%9C%A8%E5%BC%95%E8%84%9A%E7%9A%84%E5%BC%80%E5%85%B3%E4%B9%8B%E9%97%B4%E8%AE%BE%E7%BD%AE%E4%B8%80%E4%BA%9B%E5%BB%B6%E8%BF%9F%EF%BC%8C%E4%BD%BF%20LED%20%E4%BA%A7%E7%94%9F%E9%97%AA%E7%83%81%E6%95%88%E6%9E%9C%E3%80%82%E5%BB%B6%E8%BF%9F%E6%97%B6%E9%97%B4%E8%A6%81%E8%AE%BE%E7%BD%AE%E5%BE%97%E8%B6%B3%E5%A4%9F%E9%95%BF%EF%BC%8C%E4%BB%A5%E4%BE%BF%E8%83%BD%E5%A4%9F%E8%A2%AB%E5%AF%9F%E8%A7%89%E3%80%82%3CBR%20%2F%3E%3C%2FSPAN%3E%0A%3COL%20class%3D%22lia-list-style-type-lower-alpha%22%3E%0A%3CLI%3E%3CSPAN%3E%E6%B7%BB%E5%8A%A0%E8%A1%8C%E4%BB%A5%E5%88%9D%E5%A7%8B%E5%8C%96%E5%8F%98%E9%87%8F%3CBR%20%2F%3Euint8%20i%20%3D%200%3B%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%3CSPAN%3E%3CSPAN%3E%E6%9B%B4%E6%94%B9%E6%8F%90%E4%BE%9B%E7%9A%84%20%3CSTRONG%3Efor%20%3C%2FSTRONG%3E%E5%BE%AA%E7%8E%AF%E4%B8%AD%E7%9A%84%E4%BB%A3%E7%A0%81%EF%BC%8C%E5%B9%B6%E6%B7%BB%E5%8A%A0%E4%BB%A5%E4%B8%8B%E5%87%A0%E8%A1%8C%EF%BC%9A%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%0A%3CP%3E%3CBR%20%2F%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%20color%3D%22%23008000%22%3E%2F%2FLED%E9%97%AA%E7%83%8110%E6%AC%A1%E7%9A%84%E9%80%BB%E8%BE%91%3C%2FFONT%3E%3CBR%20%2F%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%3CFONT%20color%3D%22%23800080%22%3E%3CSTRONG%3Ewhile%3C%2FSTRONG%3E%3C%2FFONT%3E%20(i%2B%2B%20%26lt%3B%2010)%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%7B%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3ESiul2_Dio_Ip_WritePin%EF%BC%88LED_%E7%AB%AF%E5%8F%A3%EF%BC%8CLED_PIN%EF%BC%8C1U%EF%BC%89%EF%BC%9B%3C%2FFONT%3E%3CBR%20%2F%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%E6%B5%8B%E8%AF%95%E5%BB%B6%E8%BF%9F%EF%BC%884000000%EF%BC%89%EF%BC%9B%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3ESiul2_Dio_Ip_WritePin%EF%BC%88LED_%E7%AB%AF%E5%8F%A3%EF%BC%8CLED_PIN%EF%BC%8C0U%EF%BC%89%EF%BC%9B%3C%2FFONT%3E%3CBR%20%2F%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%E6%B5%8B%E8%AF%95%E5%BB%B6%E8%BF%9F%EF%BC%884000000%EF%BC%89%EF%BC%9B%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%7D%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20816px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20816px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202720iDFE53E30F62EE309%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3C%2FLI%3E%0A%3C%2FOL%3E%0A%3C%2FLI%3E%0A%3CLI%3E%E5%9C%A8%E2%80%9Cmain%E2%80%9D%E5%87%BD%E6%95%B0%E4%B9%8B%E5%89%8D%EF%BC%8C%E6%B7%BB%E5%8A%A0%E4%B8%80%E4%B8%AA%E5%BB%B6%E8%BF%9F%E5%87%BD%E6%95%B0%EF%BC%8C%E5%A6%82%E4%B8%8B%E6%89%80%E7%A4%BA%EF%BC%9A%3CBR%20%2F%3E%3CBR%20%2F%3E%0A%3CP%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%3CFONT%20color%3D%22%23800080%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FFONT%3E%20%3CSTRONG%3ETestDelay%3C%2FSTRONG%3E%20%EF%BC%88%20%3CFONT%20color%3D%22%23008000%22%3Euint32%3C%2FFONT%3E%E5%BB%B6%E8%BF%9F%EF%BC%89%EF%BC%9B%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%3CFONT%20color%3D%22%23800080%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FFONT%3E%20%3CSTRONG%3ETestDelay%3C%2FSTRONG%3E%20%EF%BC%88%20%3CFONT%20color%3D%22%23008000%22%3Euint32%3C%2FFONT%3E%E5%BB%B6%E8%BF%9F%EF%BC%89%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%7B%3C%2FFONT%3E%3CBR%20%2F%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%3CFONT%20color%3D%22%23800080%22%3E%3CSTRONG%3E%E9%9D%99%E6%80%81%3C%2FSTRONG%3E%3CSTRONG%3E%E6%98%93%E5%A4%B1%E6%80%A7%3C%2FSTRONG%3E%3C%2FFONT%3E%3CFONT%20color%3D%22%23008000%22%3Euint32%3C%2FFONT%3E%E5%BB%B6%E8%BF%9F%E5%AE%9A%E6%97%B6%E5%99%A8%20%3D%200%3B%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%3CFONT%20color%3D%22%23800080%22%3E%3CSTRONG%3Ewhile%3C%2FSTRONG%3E%3C%2FFONT%3E%20(DelayTimer%3CDELAY%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%7B%3C%2FFONT%3E%3CBR%20%2F%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%E5%BB%B6%E8%BF%9F%E5%AE%9A%E6%97%B6%E5%99%A8%2B%2B%EF%BC%9B%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%7D%3C%2FFONT%3E%3CBR%20%2F%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%E5%BB%B6%E8%BF%9F%E8%AE%A1%E6%97%B6%E5%99%A8%3D0%EF%BC%9B%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%7D%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202721i94566397C2295A56%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FDELAY%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FLI%3E%0A%3CLI%3E%E6%9B%B4%E6%96%B0%20main.c%20%E9%A1%B6%E9%83%A8%E7%9A%84%20includes%20%E8%A1%8C%E4%BB%A5%E5%8C%85%E5%90%AB%E5%BA%94%E7%94%A8%E7%A8%8B%E5%BA%8F%E4%B8%AD%E4%BD%BF%E7%94%A8%E7%9A%84%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E7%9A%84%E5%A4%B4%E6%96%87%E4%BB%B6%EF%BC%9A%3CBR%20%2F%3E%3CBR%20%2F%3E%E7%A7%BB%E9%99%A4%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%3CFONT%20color%3D%22%23800080%22%3E%3CSTRONG%3E%23include%3C%2FSTRONG%3E%3C%2FFONT%3E%20%3CFONT%20color%3D%22%230000FF%22%3E%22Mcal.h%22%3C%2FFONT%3E%3C%2FFONT%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%E6%B7%BB%E5%8A%A0%3CBR%20%2F%3E%0A%3CP%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%3CFONT%20color%3D%22%23800080%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FFONT%3E%3CFONT%20color%3D%22%230000FF%22%3E%E2%80%9CSiul2_Port_Ip.h%E2%80%9D%3C%2FFONT%3E%3C%2FFONT%3E%3CBR%20%2F%3E%20%3CFONT%20face%3D%22courier%20new%2Ccourier%22%20color%3D%22%23800080%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FFONT%3E%3CFONT%20color%3D%22%230000FF%22%3E%3CFONT%20face%3D%22courier%20new%2Ccourier%22%3E%E2%80%9CSiul2_Dio_Ip.h%E2%80%9D%3C%2FFONT%3E%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20524px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20524px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202722i9D152C18F5786B82%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FLI%3E%0A%3CLI%3E%E6%9E%84%E5%BB%BA%20%E2%80%9CBlinking_LED_RTD_No_AUTOSAR%E2%80%9D%E3%80%82%E5%9C%A8%20%E2%80%9CC%2FC%2B%2B%20Projects%E2%80%9D%20%E8%A7%86%E5%9B%BE%E4%B8%AD%E9%80%89%E6%8B%A9%E9%A1%B9%E7%9B%AE%E5%90%8D%E7%A7%B0%EF%BC%8C%E7%84%B6%E5%90%8E%E6%8C%89%E4%B8%8B%20%E2%80%9CBuild%E2%80%9D%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20451px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20451px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202723i8794006714A358C2%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E6%9E%84%E5%BB%BA%E5%AE%8C%E6%88%90%E5%90%8E%EF%BC%8C%E6%A3%80%E6%9F%A5%E6%98%AF%E5%90%A6%E6%9C%89%E9%94%99%E8%AF%AF%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20928px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20928px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202724i5829C4411E175AE4%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E6%89%93%E5%BC%80%20%E2%80%9CDebug%20Configurations%E2%80%9D%20%E5%B9%B6%E9%80%89%E6%8B%A9%20%E2%80%9CBlinking_LED_RTD_No_AUTOSAR_Debug_RAM%E2%80%9D%E3%80%82%E7%A1%AE%E4%BF%9D%E9%80%89%E6%8B%A9%E4%B8%8E%E6%89%A7%E8%A1%8C%E7%9A%84%E6%9E%84%E5%BB%BA%E7%B1%BB%E5%9E%8B%E5%8C%B9%E9%85%8D%E7%9A%84%E9%85%8D%E7%BD%AE%EF%BC%8C%E5%90%A6%E5%88%99%E5%A6%82%E6%9E%9C%E6%9E%84%E5%BB%BA%E8%BE%93%E5%87%BA%E4%B8%8D%E5%AD%98%E5%9C%A8%EF%BC%8C%E5%8F%AF%E8%83%BD%E4%BC%9A%E6%8A%A5%E5%91%8A%E9%94%99%E8%AF%AF%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20690px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20690px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202725i60E3DA7CA4745113%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E7%8E%B0%E5%9C%A8%EF%BC%8C%E9%9C%80%E8%A6%81%E9%80%89%E6%8B%A9%20S32%20%E8%B0%83%E8%AF%95%E6%8E%A2%E9%92%88%E6%89%80%E8%BF%9E%E6%8E%A5%E7%9A%84%E6%8E%A5%E5%8F%A3%EF%BC%88%E4%BB%A5%E5%A4%AA%E7%BD%91%E6%88%96%20USB%EF%BC%89%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20901px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20901px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202726iEBAFD68936B98001%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%0A%3COL%20class%3D%22lia-list-style-type-lower-alpha%22%3E%0A%3CLI%3E%E5%A6%82%E6%9E%9C%E9%80%9A%E8%BF%87%20USB%20%E8%BF%9E%E6%8E%A5%E4%B8%94%E9%80%89%E6%8B%A9%E4%BA%86%E6%AD%A4%E6%8E%A5%E5%8F%A3%E9%80%89%E9%A1%B9%EF%BC%8C%E5%88%99%E4%BC%9A%E8%87%AA%E5%8A%A8%E6%A3%80%E6%B5%8B%20COM%20%E7%AB%AF%E5%8F%A3%EF%BC%88%E5%9C%A8%E6%9E%81%E5%B0%91%E6%95%B0%E6%83%85%E5%86%B5%E4%B8%8B%EF%BC%8C%E5%A6%82%E6%9E%9C%E6%9C%89%202%20%E4%B8%AA%E6%88%96%E6%9B%B4%E5%A4%9A%20S32%20%E8%B0%83%E8%AF%95%E6%8E%A2%E9%92%88%E9%80%9A%E8%BF%87%20USB%20%E8%BF%9E%E6%8E%A5%E5%88%B0%E4%B8%BB%E6%9C%BA%20PC%EF%BC%8C%E5%8F%AF%E8%83%BD%E9%9C%80%E8%A6%81%E9%80%89%E6%8B%A9%E5%93%AA%E4%B8%AA%20COM%20%E7%AB%AF%E5%8F%A3%E5%AF%B9%E5%BA%94%E8%BF%9E%E6%8E%A5%E5%88%B0%E8%AF%84%E4%BC%B0%E6%9D%BF%E7%9A%84%E6%8E%A2%E9%92%88%EF%BC%89%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20952px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20952px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202727i3DA4A9AA2BF5BC4D%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3CLI%3E%E5%A6%82%E6%9E%9C%E9%80%9A%E8%BF%87%E4%BB%A5%E5%A4%AA%E7%BD%91%E8%BF%9E%E6%8E%A5%EF%BC%8C%E8%BE%93%E5%85%A5%E6%8E%A2%E9%92%88%E7%9A%84%20IP%20%E5%9C%B0%E5%9D%80%E3%80%82%E6%9C%89%E5%85%B3%E7%A1%AE%E5%AE%9A%20IP%20%E5%9C%B0%E5%9D%80%E7%9A%84%E6%96%B9%E6%B3%95%EF%BC%8C%E8%AF%B7%E5%8F%82%E9%98%85%E3%80%8AS32%20%E8%B0%83%E8%AF%95%E6%8E%A2%E9%92%88%E7%94%A8%E6%88%B7%E6%89%8B%E5%86%8C%E3%80%8B%E3%80%82%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20948px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20948px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202728iD562B9CF4EBB2FF4%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FLI%3E%0A%3C%2FOL%3E%0A%3C%2FLI%3E%0A%3CLI%3E%E7%82%B9%E5%87%BB%20%3CSTRONG%3E%E2%80%9CDebug%E2%80%9D%3C%2FSTRONG%3E%3C%2FLI%3E%0A%3CLI%3E%E8%A6%81%E6%9F%A5%E7%9C%8B%20LED%20%E9%97%AA%E7%83%81%EF%BC%8C%3CSTRONG%3E%E8%AF%B7%E5%8D%95%E5%87%BB%E2%80%9C%E6%81%A2%E5%A4%8D%E2%80%9D%E3%80%82%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20262px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22image.png%22%20style%3D%22width%3A%20262px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F202729i0F95F94457681F05%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22image.png%22%20alt%3D%22image.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3Eimage.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3C%2FLI%3E%0A%3CLI%3E%E6%AD%A4%E4%BB%A3%E7%A0%81%E5%B0%86%E4%BD%BF%20LED%20%E9%97%AA%E7%83%81%2010%20%E6%AC%A1%EF%BC%8C%E6%82%A8%E5%8F%AF%E4%BB%A5%E6%9B%B4%E6%94%B9%E5%BE%AA%E7%8E%AF%E6%9D%A1%E4%BB%B6%E4%BB%A5%E4%BD%BF%E5%85%B6%E6%97%A0%E9%99%90%E9%97%AA%E7%83%81%E3%80%82%3C%2FLI%3E%0A%3C%2FOL%3E%0A%3C%2FLINGO-BODY%3E
无评分
版本历史
最后更新:
‎06-20-2024 03:16 AM
更新人: