HOWTO: Change Vision SDK root in S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HOWTO: Change Vision SDK root in S32DS

HOWTO: Change Vision SDK root in S32DS

The Vision SDK root is contributed to the Design Studio as a dynamic path variable “S32DS_VSDK_DIR”.

Several Design Studio services use this variable to access the resources inside the Vision SDK.

By default, this variable points to “${eclipse_home}../S32DS/s32v234_sdk”, i.e. to the Vision SDK shipment bundled with Design Studio.

Technically you can change this variable to point to another instance of Vision SDK using the following steps:

1. Go to the main menu "Window -> Preferences"

pastedImage_1.png

2. Filter the preference dialog with "sub" keyword or just navigate to "Run/Debug -> String Substitution node.

pastedImage_3.png

3. Edit Variable "S32DS_VSDK_DIR" to assign another value to be substituted as Vision SDK root

pastedImage_4.png

4. Press OK when changes are complete.

評価なし
バージョン履歴
最終更新日:
‎03-05-2019 08:31 AM
更新者: