pb free

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,405件の閲覧回数
Eric_t
Contributor III

Hi,

 

We are using MC9S12DG256 controllers.

Recently we have bought a quantity from a distributor with manufacture date of 2006.

Unfortunately the package of distributor does not mention anything about pb free.

 

The package information are:

MC9S12DG256CFUE

0L91N

QQGU0622

 

Does anyone know if the above, gives any information about pb free.

I have search at freescale web site but I could not find anything.

 

Thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
2,166件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Eric,

Yes, MC9S12DG256CFUE is pb free part.

If I remember correctly E at end of part name was added for marking PB free parts.

For more details, please look at:

http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=MC9S12DG256CFUE

Note: Freescale products marked with a Lead (Pb) Free symbol meet the following definition, "Electrical and electronic assemblies and components in which the Lead (Pb) level in any of the homogeneous materials and the end product is less than 0.1% by weight."


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,167件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Eric,

Yes, MC9S12DG256CFUE is pb free part.

If I remember correctly E at end of part name was added for marking PB free parts.

For more details, please look at:

http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=MC9S12DG256CFUE

Note: Freescale products marked with a Lead (Pb) Free symbol meet the following definition, "Electrical and electronic assemblies and components in which the Lead (Pb) level in any of the homogeneous materials and the end product is less than 0.1% by weight."


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,166件の閲覧回数
Eric_t
Contributor III

Thank you RadekS

0 件の賞賛
返信