mm9z1j638 Sleep wake problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mm9z1j638 Sleep wake problem

跳至解决方案
2,856 次查看
cui1
Contributor II

hello !

I was debugging the sleep wake function and found that the program reset and run after MUC wake up, please ask whether the wake up function is normal. This is true for both sleep and stop modes.

0 项奖励
回复
1 解答
2,831 次查看
Q_man
NXP Employee
NXP Employee

There are two low power modes STOP and SLEEP mode. In SLEEP mode the wakeup behaves like a Reset for the uC.

Q_man_0-1711627585832.png

 

在原帖中查看解决方案

3 回复数
2,832 次查看
Q_man
NXP Employee
NXP Employee

There are two low power modes STOP and SLEEP mode. In SLEEP mode the wakeup behaves like a Reset for the uC.

Q_man_0-1711627585832.png

 

2,467 次查看
cui1
Contributor II
hello Q_man
Please check the stop mode and sleep mode, which mode will clear the RAM cache
0 项奖励
回复
2,837 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Due to limited resources, we are currently unable to support customers writing from generic email accounts such as gmail.com or qq.com or similar. Please ensure that you use your company email address when communicating with NXP so that we can prioritize your question accordingly.

Thank you for your understanding.

 

Regards,

Daniel

0 项奖励
回复