mm9z1j638 Sleep wake problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mm9z1j638 Sleep wake problem

ソリューションへジャンプ
2,903件の閲覧回数
cui1
Contributor II

hello !

I was debugging the sleep wake function and found that the program reset and run after MUC wake up, please ask whether the wake up function is normal. This is true for both sleep and stop modes.

0 件の賞賛
返信
1 解決策
2,878件の閲覧回数
Q_man
NXP Employee
NXP Employee

There are two low power modes STOP and SLEEP mode. In SLEEP mode the wakeup behaves like a Reset for the uC.

Q_man_0-1711627585832.png

 

元の投稿で解決策を見る

3 返答(返信)
2,879件の閲覧回数
Q_man
NXP Employee
NXP Employee

There are two low power modes STOP and SLEEP mode. In SLEEP mode the wakeup behaves like a Reset for the uC.

Q_man_0-1711627585832.png

 

2,514件の閲覧回数
cui1
Contributor II
hello Q_man
Please check the stop mode and sleep mode, which mode will clear the RAM cache
0 件の賞賛
返信
2,884件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Due to limited resources, we are currently unable to support customers writing from generic email accounts such as gmail.com or qq.com or similar. Please ensure that you use your company email address when communicating with NXP so that we can prioritize your question accordingly.

Thank you for your understanding.

 

Regards,

Daniel

0 件の賞賛
返信