mc9s12dt256b drawing too much current?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mc9s12dt256b drawing too much current?

1,324 次查看
Franklin
Contributor I
Hello,

I am powering my hcs12 through the 2.1 mm barrel connector, and have it protected by a 250 mA fuse. The manual says not to power external circuitry with more than 250 mA. I have most of the GPIO pins and PWM pins sending signals, but nothing that requires any substantial power. Port A, and T are being used to control external ICs (quadrature encoder counter chips, and the motor drivers) and 4 of the PWM pins are being used to control my motor drivers. For some reason, my fuse keeps blowing. The microcontroller is drawing more than 250mA. Is it possible that this is a result of "normal" operation? Or is my problem more likely bad wiring somewhere.

Note: The serial port is also being used to send and receive messages and a couple of the other pins (J6, J7) are being used to read switches' values.

-Concerned in Toronto
标签 (1)
0 项奖励
回复
1 回复

651 次查看
kef
Specialist I
Didn't you connect some of voltage regulator outputs (VDDPLL, VDD1, VDD2) to 5V? That could explain why so much current.
0 项奖励
回复