interrupt numbers with MC9S12XEP100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

interrupt numbers with MC9S12XEP100

Jump to solution
1,573 Views
utwig
Contributor III

Hi!

 

I am learning to use the MC9S12XEP100 with a evaluation board. I'm trying to use an interrupt to light two LEDs on the board. Whenever I interrupt the system via port P the microcontroller crashes and debugger says ILLEGAL_BP. I assume that this is due to using wrong interrupt number on the interrupt handler function.

 

I have tried these interrupt handler declarations (the two first ones compile ok):

interrupt (IVBR+Vportp) void PP0_ISR(void) {...
interrupt (IVBR+0x008E) void PP0_ISR(void) {

interrupt (0xFF8E) void PP0_ISR(void)

interrupt (0xFF00+Vportp) void PP0_ISR(void) {...

interrupt (VectorNumber_Vportp) void PP0_ISR(void) {...

 

With the debugger I can see that the I flag in CCR gets set when I interrupt port P, but the program does not go to my interrupt handler. Instead it goes to an endless loop and crashes. I have used the interrupt vector locations table on

MC9S12XEP100 Reference Manual to determine the interrupt number for the handler. But they don't work. Or there is something else wrong in my interrupt handler declarations.

 

Here's the whole code for my program:

 

#include <hidef.h>      /* common defines and macros */
#include "MC9S12XEP100.h"      /* derivative-specific definitions */

void PeriphInit(void) {
  __asm SEI;
 
  //Configures PB[0..3] as output, PB[4..7] as input
  PORTB = 0x00;           //Initialize to 0
  DDRB = 0x0F;
 
  // Enables pull-ups on PB port to drive the LEDs
   PUCR |= 0x02;
    
  //Interrupt module configuration:
  //Set the 8 address window of Interrupt Request Configuration Address Register
  //(INT_CFADDR) to base + 0x8E
  INT_CFADDR = 0x80;
 
  //base + 0x80
  INT_CFDATA0 = 0x00;
  //base + 0x82
  INT_CFDATA1 = 0x00;
  //base + 0x84
  INT_CFDATA2 = 0x00;
  //base + 0x86
  INT_CFDATA3 = 0x00;
  //base + 0x88
  INT_CFDATA4 = 0x00;
  //base + 0x8A
  INT_CFDATA5 = 0x00;
  //base + 0x8C
  INT_CFDATA6 = 0x00;
  //base + 0x8E, Port P interrupt
  INT_CFDATA7 = 0x06;
 
 
  //Configures PP0 as input
  PTP = 0x00;
  DDRP &= 0xFE;
    
  //Enables pull-up on PP0
  PERP |= 0x01;
  //Port P pin 0 interrupts on falling edge
  PPSP &= 0xFE;
  //Enables the Port P pin 0 to interrupt
  PIEP |= 0x01;
  //Write 1 to the interrupt flag register to clear the flag
  PIFP = 0x01;
                
  __asm CLI;
}

void main(void) {
  /* put your own code here */
        
  PeriphInit();

  for(;:smileywink: {

    PORTB = 0x00;
    if(!PORTB_PB4)
      PORTB_PB0 = 1;
    if(!PORTB_PB5)
      PORTB_PB1 = 1;
    if(!PORTB_PB6)
      PORTB_PB2 = 1;
    if(!PORTB_PB7)
      PORTB_PB3 = 1;
      
    _FEED_COP(); /* feeds the dog */
  } /* loop forever */
  /* please make sure that you never leave main */
}

interrupt (IVBR+0x008E) void PP0_ISR(void) {
    unsigned int j;
    PORTB_PB1 = 1;
    PORTB_PB2 = 1;
    //Wait...
    for(j = 0; j <= 2000; j++);

    
    //Write 1 to the interrupt flag register to clear the flag
    PIFP = 0x01;  
}


Labels (1)
0 Kudos
Reply
1 Solution
1,017 Views
kef
Specialist I

IVBR is interrupt vectors base register, you can't use it to specify ISR vector number. You need this number at compile time. IVBR is for run time. This should work

 

interrupt VectorNumber_Vportp void PP0_ISR(void) {...

 

Most likely you are using banked memory model. So you need to force ISR's to nonbanked memory:

 

#pragma CODE_SEG __NEAR_SEG NON_BANKED

interrupt VectorNumber_Vportp void PP0_ISR(void)

{

}

#pragma CODE_SEG DEFAULT

View solution in original post

0 Kudos
Reply
2 Replies
1,018 Views
kef
Specialist I

IVBR is interrupt vectors base register, you can't use it to specify ISR vector number. You need this number at compile time. IVBR is for run time. This should work

 

interrupt VectorNumber_Vportp void PP0_ISR(void) {...

 

Most likely you are using banked memory model. So you need to force ISR's to nonbanked memory:

 

#pragma CODE_SEG __NEAR_SEG NON_BANKED

interrupt VectorNumber_Vportp void PP0_ISR(void)

{

}

#pragma CODE_SEG DEFAULT

0 Kudos
Reply
1,017 Views
utwig
Contributor III

Thanks a lot! Those #pragmas fixed the code.

0 Kudos
Reply