Power up  cause UART printing to be come garbage in MC56F84789

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power up  cause UART printing to be come garbage in MC56F84789

957件の閲覧回数
EliArad
Contributor I

Hello

 

We are dealing with two kinds of problems with the new 84789 chip

 

The first,  after downloading the firmware using USB tap , the program runs correct, UART printing are seeing fine.

 

After power off\ON  , the UART printing are garbage completely.

 

The chip and the ELF\S-Record need to take care that the code was downloaded correct .

 

We checked the linker file and everything looks correct, even so , the linker does not complains about anything,

 

The second issue , could be related is that the next power up shows that the code is not running.

 

We need to re download the code using USB Tap to make it happened.

 

The UART issue happened all the time and the code not running happened few times.

 

Please contribute your help.

Appreciate.

 

Eli

ラベル(1)
0 件の賞賛
返信
1 返信

770件の閲覧回数
kef
Specialist I

I'm not familiar with 56F, but it would behave the same on other derivatives in case reset vector is not initialized.

0 件の賞賛
返信