how to program XGATE on XDP512?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to program XGATE on XDP512?

1,816件の閲覧回数
popup
Contributor I
Hello, I'm newbe to XGATE devices.How to program the XGATE?
I have a  TBDML working exactly fine on 9s12dg128.
Does XGATE need some special HW to be programmed?
 
Regards,
popup
ラベル(1)
0 件の賞賛
返信
1 返信

783件の閲覧回数
Steve
NXP Employee
NXP Employee
You do not need special hardware but you do need a device that has XGATE on it. The 9S12DG128 does not have XGATE.
XGATE is fully programmable in C so you don't have to learn a new language. The best place to start is with a project template from CodeWarrior or Cosmic. You can learn about how to configure the interrupts to go to XGATE and how to have XGATE handle them by reading any of the XGATE LIbrary app notes or AN3144 for a simple project example. You can also search this forum for more user examples.
0 件の賞賛
返信