about the maximum allowed continuous current of S12ZVL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

about the maximum allowed continuous current of S12ZVL

跳至解决方案
1,375 次查看
ikkishingu
Contributor II

Hello,

 

In S12ZVL Reference Manual,

Maximum allowed continuous current on PP1, PP3 and PP5 is specified -20 ~ 10mA as I_EVDD.

Which understanding is correct about this I_EVDD?

- I_EVDD is the spec for each port

or

- I_EVDD is the spec of the current sum of PP1, PP3 and PP5

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,198 次查看
DPB
NXP Employee
NXP Employee

Hello

The S12ZVL Reference Manual has not yet been released, so it is not clear exactly which information you are referring to.

However to clarify a few points.

PP1, PP3 and PP5 are not EVDD pins. PP1, PP3 and PP5 have increased current driving capability to VSSX ground.

PP7 is the EVDD1 pin which has increased current driving capability to VDDX.

The EVDD1 specification has a range of -20mA to +10mA for that pin.

The PP1,PP3 and PP5 spec. maximum is +25mA for each pin.

The total maximum current of 80mA (absolute maximum ratings) must also be taken into consideration.

The first official reference manual shall be published soon.

DPB

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,199 次查看
DPB
NXP Employee
NXP Employee

Hello

The S12ZVL Reference Manual has not yet been released, so it is not clear exactly which information you are referring to.

However to clarify a few points.

PP1, PP3 and PP5 are not EVDD pins. PP1, PP3 and PP5 have increased current driving capability to VSSX ground.

PP7 is the EVDD1 pin which has increased current driving capability to VDDX.

The EVDD1 specification has a range of -20mA to +10mA for that pin.

The PP1,PP3 and PP5 spec. maximum is +25mA for each pin.

The total maximum current of 80mA (absolute maximum ratings) must also be taken into consideration.

The first official reference manual shall be published soon.

DPB

0 项奖励
回复
1,198 次查看
ikkishingu
Contributor II

DPB-san,

Thank you for your helpful information.

It makes sense to me. I can understand clearly!!

Ikki

0 项奖励
回复