Windows emulator/simulator for S12Z devices - Unity testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows emulator/simulator for S12Z devices - Unity testing

1,672 Views
lukaleban
Contributor I

Hello,

Did anyone already try to set up a unit test framework on windows for S12Z devices?

My problem is that i cannot find an emulator to run S12Z compiled code on windows and i want to avoid using real hardware to perform unit tests on my code.

( I could compile it and run the code with GCC, but then the code is compiled with another compiler and the test lose its intention)

Any suggestion/solution would be appreciated

Best regards, Luka

0 Kudos
Reply
1 Reply

1,522 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Luka,

Unfortunately, the CodeWarrior for the S12Z devices does not support full chip simulation.
I have tried to search some tools and the second most used IDE for S12Z is probably Cosmic:
http://www.cosmic-software.com/s12z_des.php

There is a ZAP debugger. The ZAP is available in 2 execution versions for the S12Z.

1. ZAP SIM Debugger with included processor Simulator

2. ZAP BDM debugger/flash programmer uses the S12Z on-chip background debug mode


I suppose that could be a possible option, but I don’t have any experience with such tools.

Best Regards,

Diana

0 Kudos
Reply