Which Programmer?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which Programmer?

1,600件の閲覧回数
janbauer
Contributor I

Hello,

I have to programming following devices:  MC9S12ZVL64F0MLF and MC9S12ZVL96F0MLF.

Which Programmer should I take? We want to use it in the production line.

Are the CYCLONEMAX, U-CYCLONE or U-CYCLONE-FX programmer suppor this devices?

Regards Jan

ラベル(1)
0 件の賞賛
返信
1 返信

1,444件の閲覧回数
martynek
Contributor II

Hi,

Cyclone Max doesn't support S12Z programming. There is Cyclone Pro instead.

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=1&productTab=1

Please note that while the Cyclone Pro will be available until the middle of 2017, it has been replaced by the Cyclone Universal and Cyclone Universal FX production programmers. These programmers support all of the devices supported by Cyclone Pro and are recommended for new programming projects.

For more information and comparison between those two products visit: http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320165&productTab=1

Although the Cyclone Universal FX is faster, the programming speed should depend rather on a specific MCU.

Regards,

Daniel Martynek

0 件の賞賛
返信