Regarding motor commutation for S12ZVML128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding motor commutation for S12ZVML128

1,234 Views
pratibhasurabhi
Contributor V

I have to rotate motor for S12ZVML128 in open loop.I have configured the PMF,TIM,ADC.Tell me the configuration for the motor commutation.Is it necessary to set PTUC_PTULDOK bit to 1 for motor commutation?

Labels (1)
0 Kudos
Reply
1 Reply

995 Views
RadekS
NXP Employee
NXP Employee

Hi Pratibha,

The load okay bit, LDOK, enables loading the PWM generator with:

  • A prescaler divisor—from the PRSC bits in PMFFQC register
  • A PWM period—from the PWM counter modulus registers
  • A PWM pulse width—from the PWM value registers

 

We typically do not update prescaler, period or duty during open loop mode. So, we do not need to PTUC_PTULDOK bit to 1 for motor commutation.

 

The motor commutation is typically managed by TIM0_OC0 event. See Table 1-21. Control Loop Events in RM. So, we may for example invoke commutation by:

TIM0CFORC_FOC0 = 1; // force commutation event (apply first commutation sector)

The next commutation events are managed by TIM0TC0 register update. For example:

TIM0TC0 = TIM0TCNT + NextCmtPeriod;

Or

TIM0TC0 = timeCommutation + NextCmtPeriod;              // alignment + open loop

 

The PMF output signals are generated by per PMFCFG2, PMFOUTC_OUTCTL update in every commutation event (TC0 ISR). For example:

PMFCFG2 = 0x40 + MaskVal[NextCmtSector];                   // will be applied at the next commutation

PMFOUTC_OUTCTL = OutCtl[NextCmtSector];                  // will be applied at the next commutation

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply