Where can I find header files with register definitions for S12XF512 ADC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where can I find header files with register definitions for S12XF512 ADC?

1,979 次查看
lowpy
Contributor I

I need to use the ADC of the MC9S12XDP512 microcontroller. I got the example projects for the EVB9S12XF512 evaluation boards that I am using but they do not contain any headers with register definitions for ADC. My CodeWarrior (5.1) installation also does not have any headers for this derivative.

I could write my own but I wanted to check first if there is a place to get header files with register definitions for various S12 derivatives. So is there a way to find these headers or generate them automatically?

Thank you in advance!

标记 (3)
0 项奖励
回复
3 回复数

1,860 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

I have tried to create the S12XF512 project in CW 5.1 without any problem and I can see the mc9s12x512.h file in the Includes folder.

I assume that the install updates for the CW 5.1 should help.

Please open below link and click on the Previous button -> 5.1  link

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-H12-PROED-EX 

I hope it helps you. If not, let me know.

Best Regards,

Diana

0 项奖励
回复

1,860 次查看
lowpy
Contributor I

Hello Diana,

Thanks for your reply. I checked the indicated page but there are several updates for CW 5.1:

 - one compiler update

 - one processor expert update

 - several service packs for various other chips.

Which of these should I install?

Thanks again.

0 项奖励
回复

1,860 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

The fastest way will be install CodeWarrior v5.1 again.

After that, you should see the MCU in the new project window: 

pastedImage_1.png

I would like to mention that the CW v5.1 is not supported by Windows 8 or 10.

I hope it helps you.

Best Regards,

Diana

0 项奖励
回复