Where can I find header files with register definitions for S12XF512 ADC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find header files with register definitions for S12XF512 ADC?

1,954件の閲覧回数
lowpy
Contributor I

I need to use the ADC of the MC9S12XDP512 microcontroller. I got the example projects for the EVB9S12XF512 evaluation boards that I am using but they do not contain any headers with register definitions for ADC. My CodeWarrior (5.1) installation also does not have any headers for this derivative.

I could write my own but I wanted to check first if there is a place to get header files with register definitions for various S12 derivatives. So is there a way to find these headers or generate them automatically?

Thank you in advance!

タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,835件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

I have tried to create the S12XF512 project in CW 5.1 without any problem and I can see the mc9s12x512.h file in the Includes folder.

I assume that the install updates for the CW 5.1 should help.

Please open below link and click on the Previous button -> 5.1  link

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-H12-PROED-EX 

I hope it helps you. If not, let me know.

Best Regards,

Diana

0 件の賞賛
返信

1,835件の閲覧回数
lowpy
Contributor I

Hello Diana,

Thanks for your reply. I checked the indicated page but there are several updates for CW 5.1:

 - one compiler update

 - one processor expert update

 - several service packs for various other chips.

Which of these should I install?

Thanks again.

0 件の賞賛
返信

1,835件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

The fastest way will be install CodeWarrior v5.1 again.

After that, you should see the MCU in the new project window: 

pastedImage_1.png

I would like to mention that the CW v5.1 is not supported by Windows 8 or 10.

I hope it helps you.

Best Regards,

Diana

0 件の賞賛
返信