What is the difference between S12X and S12Z core ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between S12X and S12Z core ?

1,622 Views
ameykhatavkar
Contributor III

I wanted to know the difference between the S12X and S12Z core. If the things are implemented in the MCS12XDP512 can directly compatible with MC9S12ZVM.

Is there things that to be needs to be taken care before porting. Iam going through the stuffs available on this but I need immediate inputs on this.

Labels (1)
0 Kudos
Reply
1 Reply

1,138 Views
RadekS
NXP Employee
NXP Employee

Hi Amey,

Please look at my answer here:

https://community.freescale.com/message/604458#604458

I would like to add two more specific points:

1. S12Z MCUs have implemented ECC on RAM and Flash (you cannot use cumulative write into Flash).

2. Double bit ECC error, illegal opcode and illegal address access will cause Machine exception interrupt.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply