Vref of boost , current limit of boost convertor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vref of boost , current limit of boost convertor

ソリューションへジャンプ
2,933件の閲覧回数
NoahXu
Contributor III

what is the voltage value of vref of boost convertor of S12ZVML64?

what is the unit of boost convertor current limit? mA or A? hwow to set by write register value?

NoahXu_0-1705410671024.png

NoahXu_1-1705410768661.png

 

 

0 件の賞賛
返信
1 解決策
2,889件の閲覧回数
NoahXu
Contributor III
0 件の賞賛
返信
4 返答(返信)
2,919件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @NoahXu,

The Vref does not matter, there is the VSUP boost turn on/off point specified in the RM.

danielmartynek_0-1705496368662.png

 

Refer to AN5207 Hardware Design Guidelines for S12ZVM

https://www.nxp.com/webapp/Download?colCode=AN5207

There is an example.

I_out is the expected I_SUP current in your application.

 

Regards,

Daniel

 

 

0 件の賞賛
返信
2,914件の閲覧回数
NoahXu
Contributor III

Hi, Daniel

thanks,  i test and find you are right about the boost switch on /off voltage.

but i have a problem is the nosie of the inductor, the lower the vsup voltage is , the louder the noise of the inductor. 

which value should i config to eliminate the nosie?

the parameter of the circuit is atatched.

NoahXu_0-1705569606958.png

 

0 件の賞賛
返信
2,906件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @NoahXu,

Around the turn on/off point, the boot converter won't be constantly switching.

Then, it depends on many factors.

Have a look at the attached presentation, slides 23-28.

 

Regards,

Daniel

0 件の賞賛
返信
2,890件の閲覧回数
NoahXu
Contributor III

ok, thank you .

0 件の賞賛
返信