Vref of boost , current limit of boost convertor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vref of boost , current limit of boost convertor

跳至解决方案
2,791 次查看
NoahXu
Contributor III

what is the voltage value of vref of boost convertor of S12ZVML64?

what is the unit of boost convertor current limit? mA or A? hwow to set by write register value?

NoahXu_0-1705410671024.png

NoahXu_1-1705410768661.png

 

 

0 项奖励
回复
1 解答
2,747 次查看
NoahXu
Contributor III
0 项奖励
回复
4 回复数
2,777 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @NoahXu,

The Vref does not matter, there is the VSUP boost turn on/off point specified in the RM.

danielmartynek_0-1705496368662.png

 

Refer to AN5207 Hardware Design Guidelines for S12ZVM

https://www.nxp.com/webapp/Download?colCode=AN5207

There is an example.

I_out is the expected I_SUP current in your application.

 

Regards,

Daniel

 

 

0 项奖励
回复
2,772 次查看
NoahXu
Contributor III

Hi, Daniel

thanks,  i test and find you are right about the boost switch on /off voltage.

but i have a problem is the nosie of the inductor, the lower the vsup voltage is , the louder the noise of the inductor. 

which value should i config to eliminate the nosie?

the parameter of the circuit is atatched.

NoahXu_0-1705569606958.png

 

0 项奖励
回复
2,764 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @NoahXu,

Around the turn on/off point, the boot converter won't be constantly switching.

Then, it depends on many factors.

Have a look at the attached presentation, slides 23-28.

 

Regards,

Daniel

0 项奖励
回复
2,748 次查看
NoahXu
Contributor III

ok, thank you .

0 项奖励
回复