Using 1 MB flash with processor expert configuration in HCS12x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using 1 MB flash with processor expert configuration in HCS12x

2,902 次查看
mandarsansare
Contributor I

Hello,

In my projects I am using MC9S12XEP100 . I am using Processor expert mode. 

What is the maximum size of code I can compile? 

Is it possible to use code more the 64K without any additional modifications?

0 项奖励
回复
3 回复数

2,795 次查看
mandarsansare
Contributor I

What are the diffrences between

1.C compiler and C source-level debugger–code and data size restricted to 64 KB

and

2. C compiler and C source-level debugger for our XGATE module—code and data size restricted to 512 KB.

0 项奖励
回复

2,795 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

I would like to add a description from the RM v.1.25.

"The MC9S12XE-Family features an enhanced version of the performance-boosting XGATE co-processor which is programmable in “C” language."

The reduced code size for the Basic Suite means that the HCS12(X) code and data size restricted to 64K and  XGATE code and data size restricted to 512 bytes

For Standard and Professional suite is "Unlimited C compiler and C sourcelevel debugger for HCS12, HCS12X and XGATE"

Best Regards,

Diana

0 项奖励
回复

2,795 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Mandar,

The C compiler and C source-level debugger–code and data size depend on which CodeWarrior license do you use  (Free/Basic/Standard/Professional).

Please, take a look at the document below and at the S12(X) column:

https://www.nxp.com/docs/en/fact-sheet/950-00437.pdf 

The useful information for you can be that the CodeWarrior Evaluation license is based on the Professional Suite, but is time-limited usually 30 - 45 days. After that, it is a Special Edition (Free Tool).

I hope it helps you.

Best Regards,

Diana

0 项奖励
回复