Using 1 MB flash with processor expert configuration in HCS12x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using 1 MB flash with processor expert configuration in HCS12x

2,872件の閲覧回数
mandarsansare
Contributor I

Hello,

In my projects I am using MC9S12XEP100 . I am using Processor expert mode. 

What is the maximum size of code I can compile? 

Is it possible to use code more the 64K without any additional modifications?

0 件の賞賛
返信
3 返答(返信)

2,765件の閲覧回数
mandarsansare
Contributor I

What are the diffrences between

1.C compiler and C source-level debugger–code and data size restricted to 64 KB

and

2. C compiler and C source-level debugger for our XGATE module—code and data size restricted to 512 KB.

0 件の賞賛
返信

2,765件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

I would like to add a description from the RM v.1.25.

"The MC9S12XE-Family features an enhanced version of the performance-boosting XGATE co-processor which is programmable in “C” language."

The reduced code size for the Basic Suite means that the HCS12(X) code and data size restricted to 64K and  XGATE code and data size restricted to 512 bytes

For Standard and Professional suite is "Unlimited C compiler and C sourcelevel debugger for HCS12, HCS12X and XGATE"

Best Regards,

Diana

0 件の賞賛
返信

2,765件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Mandar,

The C compiler and C source-level debugger–code and data size depend on which CodeWarrior license do you use  (Free/Basic/Standard/Professional).

Please, take a look at the document below and at the S12(X) column:

https://www.nxp.com/docs/en/fact-sheet/950-00437.pdf 

The useful information for you can be that the CodeWarrior Evaluation license is based on the Professional Suite, but is time-limited usually 30 - 45 days. After that, it is a Special Edition (Free Tool).

I hope it helps you.

Best Regards,

Diana

0 件の賞賛
返信