Use CyclonePro can't unsecure issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use CyclonePro can't unsecure issue

ソリューションへジャンプ
3,227件の閲覧回数
JohnnyShih
Contributor II

Dear friend,

I had use Automotive part# S9S12G48F0MLF,

 

1. Use CyclonePro to program

2. Add security function in CyclonePro

3. But want to reprogram and unsecurity will fail.

4. If use PC & Codewarrior 5.1 & U-Multilink can to reprogram and unsecurity.

 

Pleas help check reprogram and unsecurity in Cyclone Pro (S9S12G48F0MLF).

 

Thanks a lot.


ラベル(1)
1 解決策
3,056件の閲覧回数
GordonD
Contributor IV

Johnny,

From the screen shot you supplied, I see that in the pop-up menu under the Security Settings, you have a "Generic" device selected. This setting is only for the S12 0.25u devices. For the S12G and S12P device family, which are 0.18u devices, you must select "Pxxx" from the pop-up menu. That should solve your problem.

Best Regards,

Gordon

元の投稿で解決策を見る

2 返答(返信)
3,057件の閲覧回数
GordonD
Contributor IV

Johnny,

From the screen shot you supplied, I see that in the pop-up menu under the Security Settings, you have a "Generic" device selected. This setting is only for the S12 0.25u devices. For the S12G and S12P device family, which are 0.18u devices, you must select "Pxxx" from the pop-up menu. That should solve your problem.

Best Regards,

Gordon

3,056件の閲覧回数
JohnnyShih
Contributor II

Dear Gordon,

Your suggest can fix this issue.

Thanks a lot for your support.


0 件の賞賛
返信