Use CyclonePro can't unsecure issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use CyclonePro can't unsecure issue

Jump to solution
3,367 Views
JohnnyShih
Contributor II

Dear friend,

I had use Automotive part# S9S12G48F0MLF,

 

1. Use CyclonePro to program

2. Add security function in CyclonePro

3. But want to reprogram and unsecurity will fail.

4. If use PC & Codewarrior 5.1 & U-Multilink can to reprogram and unsecurity.

 

Pleas help check reprogram and unsecurity in Cyclone Pro (S9S12G48F0MLF).

 

Thanks a lot.


Labels (1)
1 Solution
3,196 Views
GordonD
Contributor IV

Johnny,

From the screen shot you supplied, I see that in the pop-up menu under the Security Settings, you have a "Generic" device selected. This setting is only for the S12 0.25u devices. For the S12G and S12P device family, which are 0.18u devices, you must select "Pxxx" from the pop-up menu. That should solve your problem.

Best Regards,

Gordon

View solution in original post

2 Replies
3,196 Views
GordonD
Contributor IV

Johnny,

From the screen shot you supplied, I see that in the pop-up menu under the Security Settings, you have a "Generic" device selected. This setting is only for the S12 0.25u devices. For the S12G and S12P device family, which are 0.18u devices, you must select "Pxxx" from the pop-up menu. That should solve your problem.

Best Regards,

Gordon

3,196 Views
JohnnyShih
Contributor II

Dear Gordon,

Your suggest can fix this issue.

Thanks a lot for your support.


0 Kudos
Reply