Upgrade problem(Old OSJTAG/OSBDM firmware),need jump 2-pin bootloader header(JM60 IRQ to GND) on a VLG M9S12zvc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Upgrade problem(Old OSJTAG/OSBDM firmware),need jump 2-pin bootloader header(JM60 IRQ to GND) on a VLG M9S12zvc

跳至解决方案
2,339 次查看
kevinphilllips
Contributor I

need jump 2-pin bootloader header(JM60 IRQ to GND) on a VLG M9S12zvc but im not knowing where is this 2-pin jumper, and i cant do nothing until i fix it,

 

maybe is it a software solution or a good hardware schematic ?

 

thanks you all in advance !

标签 (1)
1 解答
2,076 次查看
iggi
NXP Employee
NXP Employee

Hi,

Here is the schematic of the demo board:

  VLG-MC9S12ZVC Board Schematics (REV B) 

See the sheet 7 of 13 titled OSBDM. There si the J36 jumper and it should be the one you need.

Regards,

iggi

在原帖中查看解决方案

2 回复数
2,077 次查看
iggi
NXP Employee
NXP Employee

Hi,

Here is the schematic of the demo board:

  VLG-MC9S12ZVC Board Schematics (REV B) 

See the sheet 7 of 13 titled OSBDM. There si the J36 jumper and it should be the one you need.

Regards,

iggi

2,076 次查看
kevinphilllips
Contributor I

That's work perfectly thanks you very much !

0 项奖励
回复