Upgrade problem(Old OSJTAG/OSBDM firmware),need jump 2-pin bootloader header(JM60 IRQ to GND) on a VLG M9S12zvc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Upgrade problem(Old OSJTAG/OSBDM firmware),need jump 2-pin bootloader header(JM60 IRQ to GND) on a VLG M9S12zvc

ソリューションへジャンプ
1,527件の閲覧回数
kevinphilllips
Contributor I

need jump 2-pin bootloader header(JM60 IRQ to GND) on a VLG M9S12zvc but im not knowing where is this 2-pin jumper, and i cant do nothing until i fix it,

 

maybe is it a software solution or a good hardware schematic ?

 

thanks you all in advance !

ラベル(1)
1 解決策
1,264件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

Here is the schematic of the demo board:

  VLG-MC9S12ZVC Board Schematics (REV B) 

See the sheet 7 of 13 titled OSBDM. There si the J36 jumper and it should be the one you need.

Regards,

iggi

元の投稿で解決策を見る

2 返答(返信)
1,265件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

Here is the schematic of the demo board:

  VLG-MC9S12ZVC Board Schematics (REV B) 

See the sheet 7 of 13 titled OSBDM. There si the J36 jumper and it should be the one you need.

Regards,

iggi

1,264件の閲覧回数
kevinphilllips
Contributor I

That's work perfectly thanks you very much !

0 件の賞賛
返信