TRW-S12G128 Where to get the CW project for the demo code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TRW-S12G128 Where to get the CW project for the demo code

Jump to solution
1,203 Views
michthom
Contributor II

Hi!

 

i'm looking for the sources and CW mcp file for the demo code (LED and switch handling) on the TRW-S12G128 board.

 

Someone knows if this is available somewhere?

 

Thanks in advance,

 

Michel

Labels (1)
1 Solution
1,051 Views
jacoblee
Contributor I

Hi Michel,

I think you can get it from below link.

https://www.axman.com/sites/default/files/x508_FT.zip

I hope this would be the right one.

Jacob.

View solution in original post

0 Kudos
Reply
2 Replies
1,051 Views
iggi
NXP Employee
NXP Employee

Jacob provided the right thing for you.

More various CW examples you can find with appnote AN4455:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4455.pdf

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4455SW.zip

Regards,

iggi

0 Kudos
Reply
1,052 Views
jacoblee
Contributor I

Hi Michel,

I think you can get it from below link.

https://www.axman.com/sites/default/files/x508_FT.zip

I hope this would be the right one.

Jacob.

0 Kudos
Reply