TRW-S12G128 Where to get the CW project for the demo code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TRW-S12G128 Where to get the CW project for the demo code

ソリューションへジャンプ
1,278件の閲覧回数
michthom
Contributor II

Hi!

 

i'm looking for the sources and CW mcp file for the demo code (LED and switch handling) on the TRW-S12G128 board.

 

Someone knows if this is available somewhere?

 

Thanks in advance,

 

Michel

ラベル(1)
1 解決策
1,126件の閲覧回数
jacoblee
Contributor I

Hi Michel,

I think you can get it from below link.

https://www.axman.com/sites/default/files/x508_FT.zip

I hope this would be the right one.

Jacob.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,126件の閲覧回数
iggi
NXP Employee
NXP Employee

Jacob provided the right thing for you.

More various CW examples you can find with appnote AN4455:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4455.pdf

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4455SW.zip

Regards,

iggi

0 件の賞賛
返信
1,127件の閲覧回数
jacoblee
Contributor I

Hi Michel,

I think you can get it from below link.

https://www.axman.com/sites/default/files/x508_FT.zip

I hope this would be the right one.

Jacob.

0 件の賞賛
返信