Support with sample files and libraries for MSCAN and UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support with sample files and libraries for MSCAN and UART

2,210件の閲覧回数
mitesh_sirodari
Contributor I

Hello All,

I am very new to Freescale MCU series and I am willing to use it in my products as soon as possible.

I would request to get some support for some very basic questions on the same.

I am using CodeWarrior ide for software Development of my MCU MC9S12XHZ512.

I have already initialized MCU with BAsic I/Os and now would like to go ahead with CAN and UART.

Is there any library available for initializing and functioning of MSCAN directly?

Also if few reading modules ne can suggest would be greatful.

Reagards,

Mitesh

タグ(1)
3 返答(返信)

2,006件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

I have attached two examples which show use of MSCAN and SCI. These examples are written for S12XDP512 and S12XEP100 but your S12XHZ has the same modules (S12MSCANV3, S12SCIV5).

Regards,

Daniel

0 件の賞賛
返信

2,006件の閲覧回数
aaronlee
Contributor V

Hi,

I have same request. Do you have CAN & UART examples for S12ZVCA?

Regards,

Aaron

0 件の賞賛
返信

2,006件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Aaron,

You can refer to Using MSCAN on the MagniV Family (AN4975), the software of which and UART example are attached.

Regards,

Daniel